Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Wi-Fi Combo Forum Discussions

Anonymous
Not applicable

Hi!

Did anyone use multicast with FreeRTOS-LwIP,

I tried but wiced_multicast_join() function fails, when using with FreeRTOS-LwIP.

With ThreadX-NetX it works as expected.

Wireshark sniffing claims that header checksum is wrong in FreeRTOS-LwIP case, did anyone else experience this?

Regards Erik

0 Likes
1 Reply
Anonymous
Not applicable

Found 2 problems with this. First this one, in file Wiced/Network/LwIP/ver1.4.0.rc1/src/core/ipv4/ip.c line 64.

#ifndef LWIP_INLINE_IP_CHKSUM
#define LWIP_INLINE_IP_CHKSUM   1
#endif

if #define LWIP_INLINE_IP_CHKSUM   1 is set, ip header checksum for igmp join multicast is of by 0x1600

if #define LWIP_INLINE_IP_CHKSUM   0 is set, ip header checksum for igmp join multicast is correct.

Did not investigate why that is, Not yet anyways.

Second, this one, in file Wiced/Network/LwIP/wiced/tcpip.c where I think the if statement is wrong and reversed, i.e. ERR_OK means SUCCESS not ERROR. So change != to == and then it is correct.

wiced_result_t wiced_multicast_join( wiced_interface_t interface, const wiced_ip_address_t* address )
{
    uint32_t temp;

    WICED_LINK_CHECK( interface );

    temp = htonl(address->ip.v4);
    if ( igmp_joingroup( &IP_HANDLE(interface).ip_addr, (ip_addr_t*) &temp ) != ERR_OK )
    {
        return WICED_SUCCESS;
    }
    else
    {

         return WICED_ERROR;
    }
}

wiced_result_t wiced_multicast_leave( wiced_interface_t interface, const wiced_ip_address_t* address )
{
    uint32_t temp;

    WICED_LINK_CHECK( interface );

    /* call lwip stack to leave a multicast group */
    temp = htonl(address->ip.v4);
    if ( igmp_leavegroup( &wiced_ip_handle[interface].ip_addr, (ip_addr_t*) &temp ) != ERR_OK )
    {
        return WICED_SUCCESS;
    }
    else
    {
        return WICED_ERROR;
    }
}