- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi.
I am trying to verify the external flash interfaced to the BCM943341 module (WICED 3.5.2).
Here is my pin configuration:
Module Pin 9 is SPI_MOSI
Module Pin 10 is SPI_MISO
Module Pin 11 is SCLK
Module Pin 12 is Chip Select
I have repurposed test/diagnostics/spi to read the JEDEC id. I also probed using the logic analyzer and I don't see SCLK out of pin 9.
I am thinking I am have messed up my SPI platform definitions. Please pass on any test application, debug, and platform files.
Thanks!
Regards,
Manish
This is in my platform.h header file:
/* SPI flash is present */
#define WICED_PLATFORM_INCLUDES_SPI_FLASH
/* SPI Flash. Implemented by Inventek Systems ... */
#ifdef WICED_PLATFORM_INCLUDES_SPI_FLASH
//#pragma message "SPI Flash included in platform"
//#define WICED_PLATFORM_INCLUDES_SPI_FLASH
#define WICED_SPI_FLASH_CS ( WICED_GPIO_8 ) //( WICED_GPIO_21 )
#define WICED_SPI_FLASH_MOSI ( WICED_GPIO_5 ) //( WICED_GPIO_18 )
#define WICED_SPI_FLASH_MISO ( WICED_GPIO_6 ) //( WICED_GPIO_17 )
#define WICED_SPI_FLASH_CLK ( WICED_GPIO_7 )//( WICED_GPIO_19 )
#endif
This is in my platform.c header file:
#ifdef WICED_PLATFORM_INCLUDES_SPI_FLASH
/* SPI peripherals. Used for Serial FLASH */
const platform_spi_t platform_spi_peripherals[] =
{
[WICED_SPI_1] =
{
.port = SPI1,
.gpio_af = GPIO_AF_SPI1,
.peripheral_clock_reg = RCC_APB2Periph_SPI1,
.peripheral_clock_func = RCC_APB2PeriphClockCmd,
.pin_mosi = &platform_gpio_pins[WICED_SPI_FLASH_MOSI],
.pin_miso = &platform_gpio_pins[WICED_SPI_FLASH_MISO],
.pin_clock = &platform_gpio_pins[WICED_SPI_FLASH_CLK],
.tx_dma =
{
.controller = DMA2,
.stream = DMA2_Stream5,
.channel = DMA_Channel_3,
.irq_vector = DMA2_Stream5_IRQn,
.complete_flags = DMA_HISR_TCIF5,
.error_flags = ( DMA_HISR_TEIF5 | DMA_HISR_FEIF5 | DMA_HISR_DMEIF5 ),
},
.rx_dma =
{
.controller = DMA2,
.stream = DMA2_Stream0,
.channel = DMA_Channel_3,
.irq_vector = DMA2_Stream0_IRQn,
.complete_flags = DMA_LISR_TCIF0,
.error_flags = ( DMA_LISR_TEIF0 | DMA_LISR_FEIF0 | DMA_LISR_DMEIF0 ),
},
}
};
#endif
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
This is resolved now and I can read the JEDEC.