Information on Values in wifi_nvram_image.h

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
WaCu_1902616
Level 2
Level 2
First like received
Were looking for some documantaion of the values in wifi_nvram_image.h (from the WICED SDK.)  Were specifically looking at spuravoid_enable2g and loggen_mode, but wed greatly appreciate any documentation thats available!
0 Likes
3 Replies
clprc_2121281
Level 1
Level 1

Hello,

Have you received any reply on this regard?

Thanks!

0 Likes
Anonymous
Not applicable

The NVRAM variables are not to be modified unless directly instructed to do so as incorrect values can cause unpredictable damaging behaviour as well as potentially damage the device.

Why are interested in those two variables?

0 Likes

Hello nikvh

Not sure if you are asking regarding my reply or regarding wcurrier's comment. In my case, there is a board redesign and there is also a change on the Broadcom chipset. We are in the middle of validation and part of it is veryfing EVM which is not as good as expected. The intention is to update power and/or country code in order to achieve a better performance.

Thanks for your reply, nikvh

0 Likes