Hi bkkim,
FreeRTOS: is the embedded OS that can be installed on the WICED platform
LwIP: lightweight TCP/IP stack: lwIP - A Lightweight TCP/IP stack - Summary [Savannah]
SDIO: in this context, this is the bus interface between the radio chip and the host processor.
SPI: another possible bus interface between the radio chip and the host processor.
ThreadX: another OS that can be installed on the WICED platform.
NetX:IPv4 TCP/IP stack
NetX_Duo: includes both IPv4 and IPv6 TCP/IP stacks.
Hi bkkim,
FreeRTOS: is the embedded OS that can be installed on the WICED platform
LwIP: lightweight TCP/IP stack: lwIP - A Lightweight TCP/IP stack - Summary [Savannah]
SDIO: in this context, this is the bus interface between the radio chip and the host processor.
SPI: another possible bus interface between the radio chip and the host processor.
ThreadX: another OS that can be installed on the WICED platform.
NetX:IPv4 TCP/IP stack
NetX_Duo: includes both IPv4 and IPv6 TCP/IP stacks.