Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

The ota_fr test app builds but seg faults when it tries to download. I am testing with a BCM943362WCD4_3 board. When I try and integrate the ota server code into my application it seems to work with respect to running the AP mode and managing the HTTP transactions but it only intermittently reboots correctly and even when it does the code has not been written properly. I added some debug printf's and it seems that the sflash inteface is not reading/writing properly because it reads an app_header.count = 0 and this causes wiced_apps_get_physical_address() to fail, which ultimatley causes the process_upgrade_chunk() to fail, even though it's not inidicated in the WICED console output. Any help would be appreciated!

(1) Log except from my application runing the wiced OTA server(note that this log as the augmented debug output I added) :

Error#1:

============

Network ready IP: 192.168.10.1

Error setting application size!!

current_size: 0, file_size: 461632

Error setting application size!!

current_size: 0, file_size: 461632

Error setting application size!!

current_size: 0, file_size: 461632

Error setting application size!!

current_size: 0, file_size: 461632

Error setting application size!!

current_size: 0, file_size: 461632

Error setting application size!!

current_size: 0, file_size: 461632

Error setting application size!!

current_size: 0, file_size: 461632

Error setting application size!!

current_size: 0, file_size: 461632

Error setting application size!!

current_size: 0, file_size: 461632

Error setting application size!!

current_size: 0, file_size: 461632

Error#2:

============

Writing chunk 449 of size 1024 from offset 458752

wiced_apps_write: offset: 0x1800, app_header.count: 0x0

process_upgrade_chunk: Error writing chunk (err = 4)

Writing chunk 450 of size 1024 from offset 459776

wiced_apps_write: offset: 0x1800, app_header.count: 0x0

process_upgrade_chunk: Error writing chunk (err = 4)

Writing chunk 451 of size 832 from offset 460800

wiced_apps_write: offset: 0x1800, app_header.count: 0x0

process_upgrade_chunk: Error writing chunk (err = 4)

Uploaded file size = 461632

(2) Log output when trying to build and download ota_fr:

root@ubuntu:/home/confocus/WICED/WICED-SDK-3.3.0# ./make clean

Cleaning...

Done

root@ubuntu:/home/confocus/WICED/WICED-SDK-3.3.0#

root@ubuntu:/home/confocus/WICED/WICED-SDK-3.3.0#

root@ubuntu:/home/confocus/WICED/WICED-SDK-3.3.0#

root@ubuntu:/home/confocus/WICED/WICED-SDK-3.3.0# ./make snip.ota_fr-BCM943362WCD4 download download_apps run

Making config file for first time

+-----------------------------------------------------------------------------------------------------+

| IMPORTANT NOTES                                                                                     |

+-----------------------------------------------------------------------------------------------------+

| Wi-Fi MAC Address                                                                                   |

|    The target Wi-Fi MAC address is defined in <WICED-SDK>/generated_mac_address.txt                 |

|    Ensure each target device has a unique address.                                                  |

+-----------------------------------------------------------------------------------------------------+

| MCU & Wi-Fi Power Save                                                                              |

|    It is *critical* that applications using WICED Powersave API functions connect an accurate 32kHz |

|    reference clock to the sleep clock input pin of the WLAN chip. Please read the WICED Powersave   |

|    Application Note located in the documentation directory if you plan to use powersave features.   |

+-----------------------------------------------------------------------------------------------------+

Building Bootloader

Building Serial Flash Loader App

Making config file for first time

+-----------------------------------------------------------------------------------------------------+

| IMPORTANT NOTES                                                                                     |

+-----------------------------------------------------------------------------------------------------+

| Wi-Fi MAC Address                                                                                   |

|    The target Wi-Fi MAC address is defined in <WICED-SDK>/generated_mac_address.txt                 |

|    Ensure each target device has a unique address.                                                  |

+-----------------------------------------------------------------------------------------------------+

| MCU & Wi-Fi Power Save                                                                              |

|    It is *critical* that applications using WICED Powersave API functions connect an accurate 32kHz |

|    reference clock to the sleep clock input pin of the WLAN chip. Please read the WICED Powersave   |

|    Application Note located in the documentation directory if you plan to use powersave features.   |

+-----------------------------------------------------------------------------------------------------+

Compiling App_SFlash_write

Compiling Platform_BCM943362WCD4

Compiling WWD_NoOS_Interface

Compiling WWD_NoNS_Interface

Compiling Lib_SPI_Flash_Library_BCM943362WCD4

Compiling WWD_for_SDIO_NoOS

Compiling Lib_Wiced_RO_FS

Compiling STM32F2xx

Compiling Lib_TLV

Compiling common_GCC

Compiling STM32F2xx_Peripheral_Drivers

Finished Building Bootloader

Processing resources

Creating security credentials

Compiling Lib_Ring_Buffer

Compiling STM32F2xx_Peripheral_Libraries

Making DCT image

Compiling App_OTA_fr_run

Compiling Platform_BCM943362WCD4

Compiling NetX_Duo

Compiling WICED

Making waf_sflash_write-NoOS-NoNS-BCM943362WCD4-SDIO.elf

waf_sflash_write-NoOS-NoNS-BCM943362WCD4-SDIO

----------------------------------|---------|---------|

                                  |         |  Static |

              Module              |  Flash  |   RAM   |

----------------------------------+---------+---------|

App                               |       0 |   21130 |

Host MCU-family library           |       0 |   12034 |

Interrupt Vectors                 |       0 |     388 |

libc                              |       0 |     548 |

platform                          |       0 |     972 |

Ring_Buffer                       |       0 |      34 |

SPI_Flash_Library_BCM943362WCD4   |       0 |     792 |

Startup Stack & Link Script fill  |       0 |     486 |

WWD                               |       0 |     144 |

----------------------------------+---------+---------|

TOTAL (bytes)                     |       0 |   36528 |

----------------------------------|---------|---------|

Making waf_sflash_write-NoOS-NoNS-BCM943362WCD4-SDIO.bin

Build complete

Finished Building Serial Flash Loader App

Compiling Lib_OTA_Server

Compiling Lib_SPI_Flash_Library_BCM943362WCD4

Compiling WWD_ThreadX_Interface

Compiling WICED_ThreadX_Interface

Compiling WWD_NetX_Duo_Interface

Compiling WICED_NetX_Duo_Interface

Compiling Supplicant_BESL

Compiling Lib_DNS

Compiling WWD_for_SDIO_ThreadX

Compiling Lib_Wiced_RO_FS

Compiling STM32F2xx

Compiling Lib_DHCP_Server

Compiling Lib_Linked_List

Compiling Lib_base64

Compiling Lib_TLV

Compiling Lib_crypto_open

Compiling common_GCC

Compiling STM32F2xx_Peripheral_Drivers

Compiling Lib_Ring_Buffer

Compiling STM32F2xx_Peripheral_Libraries

Making snip_ota_fr-BCM943362WCD4.elf

Making snip_ota_fr-BCM943362WCD4.bin

snip_ota_fr-BCM943362WCD4

----------------------------------|---------|---------|

                                  |         |  Static |

              Module              |  Flash  |   RAM   |

----------------------------------+---------+---------|

App                               |     293 |       0 |

base64                            |     519 |       0 |

crypto_open                       |   50125 |       0 |

DHCP_Server                       |    1510 |     132 |

DNS                               |      64 |      44 |

Host MCU-family library           |   14093 |    2740 |

Interrupt Vectors                 |     388 |       0 |

libc                              |   34815 |    3136 |

Networking                        |    4534 |   14909 |

NetX-Duo - Interfaces & Stacks    |       0 |      16 |

OTA_Server                        |    8283 |     684 |

Other                             |   43276 |     535 |

Packet Buffers                    |       0 |   23142 |

platform                          |    1116 |     168 |

RAM Initialisation                |    2424 |       0 |

resources                         |      16 |       0 |

Ring_Buffer                       |      94 |       0 |

SPI_Flash_Library_BCM943362WCD4   |     760 |       0 |

Startup Stack & Link Script fill  |      63 |      10 |

Supplicant - BESL                 |   15226 |     504 |

ThreadX                           |    8612 |     396 |

Wi-Fi Firmware                    |  210412 |       0 |

WICED                             |    2840 |     616 |

WWD                               |   12957 |    1604 |

----------------------------------+---------+---------|

TOTAL (bytes)                     |  409996 |   48636 |

----------------------------------|---------|---------|

Downloading Bootloader ...

Segmentation fault (core dumped)

make: *** [main_app] Error 139

0 Likes
1 Solution

First you should replace your tools/Linux??/common/make with your system make to fixed the Segmentation fault under Linux!

Then build the ota_fr with download_apps to download the ota_fr into external flash include APPS_LUT !

View solution in original post

5 Replies
Anonymous
Not applicable

Sorry,

The module is: BCM943362WCD4_3

The eval board is: BCM943362WCD4_EVB (Rev 1)

0 Likes
Anonymous
Not applicable

Hello,

Could you make sure your makefile is as follows:

snip.ota_fr-BCM943362WCD4 download download_apps run

It is important to include "download_apps" in your makefile name.

Thanks,

Arsh Buch

0 Likes

First you should replace your tools/Linux??/common/make with your system make to fixed the Segmentation fault under Linux!

Then build the ota_fr with download_apps to download the ota_fr into external flash include APPS_LUT !

Anonymous
Not applicable

This is correct, but a little more detail would have been helpful.

0 Likes
Anonymous
Not applicable

The ota_fr demo app build fails when the 'download_apps' option is passed with Broadcom's version of make, located in this directory:

.../WICED-SDK-3.3.0/tools/common/Linux32

FIX: replace Broadcom make with the native make:

mv make make.orig && ln -s /usr/bin/make make

With the above change, the ota_fr test app can be built and downloaded correctly, even with the

download_apps option.. After ota_fr is run,, the DCT image in the external serial flash is updated with application header/location/size information which the OTA process uses. Attempts to perform OTA upgrade will now succeed from either the ota_fr test app or from a user application calling the ota server.

0 Likes