Sep 30, 2022
04:33 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Sep 30, 2022
04:33 AM
Hello.
In a previous post I read that I can use TopJTAG Flash Programmer to drive ARM-USB-TINY-H From Olimex, so
I've bought ARM-USB-TINY-H and I've downloaded TopJTAG Flash Programmer for evaluation.
I've installed TopJTAG Flash Programmer.
After running TopJTAG Flash Programmer I went to "Setup>>JTAG Connection".
In this window I selected "Connection: Generic FTDI FT2232" and "Static pins: Olimex ARM-USB-OCD".
But, when I click the green refresh button at the right of "Static pins", the software doesn't see the attached ARM-USB-TINY-H From Olimex
My machine is Windows 10 Pro 64x and in the device manager I see my ARM-USB-TINY-H From Olimex
to install OLIMEX I've used zadig 2.5
Labels
- Labels:
-
WICED Studio Wi-Fi Combo
- Tags:
- olimex
0 Replies