Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

JuMo_1762556
Level 3
Level 3
First like received First like given

I am using WICED-Studio-6.1 on CYW943907AEVAL1F platform.

We want to use RTS of UART0 (UART0_RTS_OUT:A53) as GPIO.

For example, please teach me how RTS is fixed to high during transmission in apps/snip/uart/uart.c .

1 Solution

On analysing further, it is found that the UART0_RTS pin can be either mapped to RTS function or disabled. But it cannot be used as GPIO. You can use any other GPIO pin such as GPIO_15 as GPIO function using the GPIO APIs discussed earlier. Ensure that the GPIO pin is not being used for any other dedicated function in the eval board.

View solution in original post

8 Replies
GauravS_31
Moderator
Moderator
Moderator
250 solutions authored 250 sign-ins First comment on KBA

If you want to use RTS of UART0 as GPIO, first check in the datasheet the pin multiplexing of UART0_RTS. It is multiplexed with GPIO_11, GPIO_7 and GPIO_15. If we select GPIO_11 for instance, check the platform pin mapping table in platform.c. The GPIO_11 is mapped to WICED_GPIO_7. In your application code, initialize the GPIO using wiced_gpio_init(WICED_GPIO_7, OUTPUT_PUSH_PULL). The second parameter in the API is pin configuration which you can modify based on your requirement.

0 Likes

Thank you for answer.

I changed the code as follows but I couldn't see the results.

I monitored J6 pin24 (UART0_RTS_OUT) of CYW943907AEVAL1F by oscilloscope.

I appreciate any helps.

/******************************************************

*               Variable Definitions

******************************************************/

wiced_uart_config_t uart_config =

{

    .baud_rate    = 115200,

    .data_width   = DATA_WIDTH_8BIT,

    .parity       = NO_PARITY,

    .stop_bits    = STOP_BITS_1,

    .flow_control = FLOW_CONTROL_DISABLED,

};

wiced_ring_buffer_t rx_buffer;

uint8_t             rx_data[RX_BUFFER_SIZE];

/******************************************************

*               Function Definitions

******************************************************/

void application_start( )

{

     char c;

     uint32_t expected_data_size = 1;

     /* Initialise ring buffer */

     ring_buffer_init(&rx_buffer, rx_data, RX_BUFFER_SIZE );

     /* Initialise UART. A ring buffer is used to hold received characters */

     wiced_uart_init( WICED_UART_2, &uart_config, &rx_buffer );

     wiced_gpio_init( WICED_GPIO_7, OUTPUT_PUSH_PULL ); /* RTS GPIO init */

     /* Send a test string to the terminal */

     wiced_gpio_output_high( WICED_GPIO_7 ); /* RTS High */

     wiced_uart_transmit_bytes( WICED_UART_2, TEST_STR, sizeof( TEST_STR ) - 1 );

     wiced_gpio_output_low( WICED_GPIO_7 ); /* RTS Low */

     /* Wait for user input. If received, echo it back to the terminal */

     while ( wiced_uart_receive_bytes( WICED_UART_2, &c, &expected_data_size, WICED_NEVER_TIMEOUT ) == WICED_SUCCESS )

     {

         wiced_gpio_output_high( WICED_GPIO_7 ); /* RTS High */

         wiced_uart_transmit_bytes( WICED_UART_2, &c, 1 );

         wiced_gpio_output_low( WICED_GPIO_7 ); /* RTS Low */

         expected_data_size = 1;

     }

}

Since UART0_RTS is to be used as GPIO, the RTS function must be disabled. Go to platform.c, [WICED_UART_2] and assign .rts_pin=NULL and .cts_pin=NULL.

0 Likes

Thank you again for your input.

I tried as you wrote but RTS didn't show High.

Any other modification is needed ?

0 Likes

Can you create a separate application to test only WICED_GPIO_7? You can output the pin high in this application for testing purpose. We need to ensure that the GPIO operation works in isolation.

  I made a program only of WICED_GPIO_7 but RTS doesn't change.

  The program is as follows;

/******************************************************

*               Function Definitions

******************************************************/

#define UART_RTS     (WICED_GPIO_7)

void application_start( )

{

#if 0

    char c;

    uint32_t expected_data_size = 1;

    /* Initialise ring buffer */

    ring_buffer_init(&rx_buffer, rx_data, RX_BUFFER_SIZE );

    /* Initialise UART. A ring buffer is used to hold received characters */

    wiced_uart_init( WICED_UART_2, &uart_config, &rx_buffer );

    wiced_gpio_init( UART_RTS, OUTPUT_PUSH_PULL ); /* RTS GPIO init */

    /* Send a test string to the terminal */

    wiced_gpio_output_high( UART_RTS ); /* RTS High */

    wiced_uart_transmit_bytes( WICED_UART_2, TEST_STR, sizeof( TEST_STR ) - 1 );

    wiced_gpio_output_low( UART_RTS ); /* RTS Low */

    /* Wait for user input. If received, echo it back to the terminal */

    while ( wiced_uart_receive_bytes( WICED_UART_2, &c, &expected_data_size, WICED_NEVER_TIMEOUT ) == WICED_SUCCESS )

    {

        wiced_gpio_output_high( UART_RTS ); /* RTS High */

        wiced_uart_transmit_bytes( WICED_UART_2, &c, 1 );

        wiced_gpio_output_low( UART_RTS ); /* RTS Low */

        expected_data_size = 1;

    }

#else /* temp */

    wiced_gpio_init( UART_RTS, OUTPUT_PUSH_PULL ); /* RTS GPIO init */

    while ( 1 )

    {

        wiced_gpio_output_high( UART_RTS ); /* RTS High */

        wiced_rtos_delay_milliseconds( 1000 );

        wiced_gpio_output_low( UART_RTS ); /* RTS Low */

    }

#endif

}

0 Likes

On analysing further, it is found that the UART0_RTS pin can be either mapped to RTS function or disabled. But it cannot be used as GPIO. You can use any other GPIO pin such as GPIO_15 as GPIO function using the GPIO APIs discussed earlier. Ensure that the GPIO pin is not being used for any other dedicated function in the eval board.

Thank you for the answer.

I understood that J6 pin24 (UART0_RTS_OUT) can't be used as GPIO.

0 Likes