- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello
How to perform receiver blocking test CYW43455(1MW) without using CMW and also command for continous RX mode
Command in which we can see PER rate or number of packet TX and RX
Thanks,
Ekta
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Eksi_4748921 ,
Please have a look at the reference links below:
Module Partner Ecosystem: Tools for Getting to Production with Certified Modules
HCI-Based Bluetooth Testing - the doc contains generic HCI commands structure as well as Bluez (hci tool ) format commands for BT RF test.
For packet error calculations :
- For BLE , you have to run HCI_LE_Receiver_Test ( OGF: 0x08 , OCF: 0x01D ) and then end the test using HCI_LE_Test_End (OGF: 0x08 , OCF: 0x01F) . Results will be provided – Number of packets
Refer to the commands and response format from the doc available here: https://community.cypress.com/docs/DOC-19558
- For BR/EDR , refer Rx_test ( OGF: 0x3F , OCF:0x052 ) , the statistics report received after the command complete event will have the packet received. Check the example in doc mentioned above
Hope this helps.
Regards,
Anjana