How to import WICED_SDK_SPIL_platform_file_2.3.1 to WICED-SDK-3.1.0

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hello all,

I made my own board equipped with SSB-WM-N01 chip and I want to download a firmware to the SSB-WM-N01 using WICED-SDK-3.1.0. Currently, I have the WICED_SDK_SPIL_platform_file_2.3.1.zip, but I don't know how to import it to WICED-SDK-3.1.0.

Please explain it with an example like snip.scan app download.

And if the import is successful, then is there any remaining work to apply the SPIL platform to my own board.

If I try to download snip.scap app to my own board, which do I have to change from the following command.

snip.scan-BCM943362WCD4 JTAG=Olimex_ARM-USB-TINY-H download run

In the mean while, I heard from the chip distributor that the SSB-WM-N01 has its own bootloader and it doesn't need jtag connection for downloading firmware. If it's right, can I download a firmware by using only UART port (not using FT2232HL-R chip) like WICED Smart module.

Best regards,

0 Likes
3 Replies
Anonymous
Not applicable

If you need it still, please contact me.

0 Likes
Anonymous
Not applicable

Dear gideonhyun,

Thanks for your response.

Fortunately, I obtained the SPIL platform file from local distributor in Korea.

Best regards,

PS: Aside from this, I’m looking for the sample code regarding interrupt based ADC control using WICED WIFI. Please let me know if you have the information on it.

Yongsun

0 Likes
Anonymous
Not applicable

Actually, we provide the module made by BCM43362 + CM4. If you have any

question for the module, let me know please. Thanks.

https://ack.me/products/AMW006_Numbat

https://ack.me/products/AMW004_Wallaby

2014-12-17 16:00 GMT+09:00 김용선 <communities-list@community.broadcom.com>:

<http://community.broadcom.com/?et=watches.email.thread> How to

import WICED_SDK_SPIL_platform_file_2.3.1 to WICED-SDK-3.1.0

reply from 김용선

<http://community.broadcom.com/people/%EA%B9%80%EC%9A%A9%EC%84%A0?et=watches.email.thread>

in WICED Wi-Fi Forums - View the full discussion

<http://community.broadcom.com/message/10919?et=watches.email.thread#10919>

0 Likes