Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

DeXi_1316761
Level 3
Level 3
5 sign-ins 10 replies posted 5 replies posted

I konw that the WICED studio support freeRTOS and ThreadX. In the project, how to configure for freeRTOS or ThreadX?

1 Solution
GauravS_31
Moderator
Moderator
Moderator
250 solutions authored 250 sign-ins First comment on KBA

You can modify or create a new make target on the right hand side of WICED Studio to include the appropriate RTOS-Network stack for your project. For FreeRTOS, the make target would be snip.scan-BCM943364WCD1-FreeRTOS-LwIP download download_apps run. For ThreadX, it would be snip.scan-BCM943364WCD1-ThreadX-NetX_Duo download download_apps run.

View solution in original post

2 Replies
GauravS_31
Moderator
Moderator
Moderator
250 solutions authored 250 sign-ins First comment on KBA

You can modify or create a new make target on the right hand side of WICED Studio to include the appropriate RTOS-Network stack for your project. For FreeRTOS, the make target would be snip.scan-BCM943364WCD1-FreeRTOS-LwIP download download_apps run. For ThreadX, it would be snip.scan-BCM943364WCD1-ThreadX-NetX_Duo download download_apps run.

Is this FreeRTOS Support all Platform files ? Because I am using ISM43340 inventek Wif/ble Combo Module. This Module working in ThreadX RTOS  mode . Whatever you mention above examples (snip.scan-ISM43340--ThreadX-NetX-download download_apps run) . There is no problem at all in ThreadX RTOS.  If I change to FreeRTOS mode. It's not working . It's went platform_mcu_reset funtion . I mean  wiced_init function getting failed. Here I those please verify it.

ThreadX logs  --- It's working in ThreadX RTOS

Starting WICED Wiced_006.004.000.0061

Platform ISM43340_M4G_L44 initialised

Started ThreadX v5.8

WICED_core Initialized

Initialising NetX v5.10_sp3

Creating Packet pools

WLAN MAC Address : C4:7F:51:8C:FB:4E

WLAN Firmware    : wl0: Nov 18 2015 20:26:53 version 6.49.1 (r600471) FWID 01-a0191015

WLAN CLM         : API: 7.2 Data: 6.2.4 Compiler: 1.9.3 ClmImport: 1.9.3 Inc Data: 9.3.7 Inc Compiler: 1.29.24 Inc ClmImport: 1.29.20

Waiting for scan results...

  # Type  BSSID              RSSI Rate Chan Security               SSID                            CCode    Flag

------------------------------------------------------------------------------------------------------------------

  0 Infra C4:71:54:0C:C5:D4 -57 300.0    1   WPA2 AES PSK         TP-Link_C5D4                             PROBE        

  1 Infra 48:EE:0C:A4:C1:E9 OFF  54.0   10   WEP PSK              D-Link                                   PROBE        

  2 Infra CC:9F:7A:99:0A:7E -57  72.2   11   WPA2 AES PSK         kasi                                     PROBE        

Scan complete in 2533 milliseconds

Waiting for scan results...

  # Type  BSSID              RSSI Rate Chan Security               SSID                            CCode    Flag

------------------------------------------------------------------------------------------------------------------

  0 Infra C4:71:54:0C:C5:D4 -57 300.0    1   WPA2 AES PSK         TP-Link_C5D4                             PROBE        

  1 Infra 00:AD:24:F6:AE:E9 OFF 300.0    7   WPA2 AES PSK         Mohan                                    BEACON       

  2 Infra 48:EE:0C:A4:C1:E9 OFF  54.0   10   WEP PSK              D-Link                                   PROBE        

  3 Infra CC:9F:7A:99:0A:7E OFF  72.2   11   WPA2 AES PSK         kasi                                     PROBE        

Scan complete in 2540 milliseconds

FreeRTOS Log

Starting WICED Wiced_006.004.000.0061

Platform ISM43340_M4G_L44 initialised

Started FreeRTOS v9.0.0

WICED_core Initialized

Initialising LwIP v2.0.3

DHCP CLIENT hostname WICED IP

After this it went system_reset.  Can you please guide me for this issue

FreeRTOS_error.PNG

0 Likes