We've received reports that CA(Certification Authority) are not being checked, and we're considering taking action.
Since "TLS_VERIFICATION_REQUIRED" is set, I think the SSL certificate verification process is working.
◆ File
wiced_defaults.h
/* WICED TLS Options * /
#define WICED_TLS_DEFAULT_VERIFICATION (TLS_VERIFICATION_REQUIRED)
◆ Environment
・ WICED SDK: 6.4.0
・ OS: ThreadX
◆makefile
In the current situation, to check the Certification Authority (CA), is it enough to set the path of the root CA to "CERTIFICATE" and "PRIVATE_KEY" in the makefile?
Or is this a self-signed certificate for the HTTP server, and there is another way to check for a Certificate Authority?
CERTIFICATE := $(SOURCE_ROOT)resources/certificates/server_cert.cer
PRIVATE_KEY := $(SOURCE_ROOT)resources/certificates/server_cert_key.key
Solved! Go to Solution.
Hi @hiko_4316286 ,
Yes, It is enough to set the path of the root CA to "CERTIFICATE" and "PRIVATE_KEY" in the makefile.
You can verify whether CERTIFICATE_STRING and PRIVATE_KEY_STRING are getting generated in generated_security_dct.h file which is present inside build folder.
And both strings will be written into DCT_SECURITY_SECTION in flash from where the code reads the strings for verification.
Thanks,
Rakesh B G
Hi @hiko_4316286 ,
Yes, It is enough to set the path of the root CA to "CERTIFICATE" and "PRIVATE_KEY" in the makefile.
You can verify whether CERTIFICATE_STRING and PRIVATE_KEY_STRING are getting generated in generated_security_dct.h file which is present inside build folder.
And both strings will be written into DCT_SECURITY_SECTION in flash from where the code reads the strings for verification.
Thanks,
Rakesh B G