Anonymous
Not applicable
Aug 19, 2013
11:20 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Aug 19, 2013
11:20 PM
# Environments- WICED Version 2.3.1- ThreadX + NetX_Duo- BCMUSI11 Platform- BCM43362Hi 🙂I would like to use wiced_wifi_join_specific function in the wiced_join_ap function.Because when there are two APs which have same SSID, I would be able to choose one of them to be joined. So I stored AP information in the stored_ap_list[0] variable in the wifi config dct and tested it,but when I called wiced_network_up function on the Infrastructure STA mode, it doesnt work at all.If there is two APs which have same SSID, one is channel 1 and another is channel 6.How can I join to channel 6 AP? (or to a AP which has specific BSSID?)RegardsMike Jeong
Labels
- Labels:
-
SPI
- Tags:
- 2.3.1
- 809912
- bcm43362
- bcmusi11
- bssid
- called
- channel
- choose
- config
- environments
- function
- information
- infrastructure
- jeong
- join
- joined
- mike
- mode
- netx_duo
- platform
- specific
- ssid
- stored
- stored_ap_list[0]
- tested
- threadx
- variable
- version
- wiced
- wiced_join_ap
- wiced_network_up
- wiced_wifi_join_specific
- wifi
- work
2 Replies
Jun 16, 2014
11:04 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jun 16, 2014
11:04 AM
Can you let us know if this is still an open issue and still an issue with SDK2.4.0?
Thank you.
Jun 27, 2014
01:34 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jun 27, 2014
01:34 PM
Hello,
Certainly suggest moving to SDK 2.4.0
To join a specific AP BSSID must be used.
An example of this is in the "console app" using the "test credentials" command.
test_cred <ssid> <bssid> <channel> <open|wep|wpa_aes|wpa_tkip|wpa2|wpa2_tkip> [key]
-