- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I am using Murata Type 1Dx module, which uses Broadcom BCM4343W chipset.
I am trying to bring-up the Bluetooth module & using WICED SDK 3.5.2
My host MCU platform is ARM Cortex M4. I am using WICED-SDK-3.5.2\apps\snip\bluetooth\ble_hello_sensor application.
I could see read/write operations happening through UART port.
On Console I see below messages
00000000 GKI_create_task func=0xfa1d id=1 name=BTU stack=0x0 stackSize=6144
00000000 GKI_create_task func=0x10e91 id=0 name=HCISU stack=0x0 stackSize=4096
00096110 GKI_exception(): Task State Table
00096110 GKI_exception 65524 getbuf: out of buffers
00100110 GKI_exception(): Task State Table
00100110 GKI_exception 65524 getbuf: out of buffers
00104110 GKI_exception(): Task State Table
00104110 GKI_exception 65524 getbuf: out of buffers
00108110 GKI_exception(): Task State Table
00108110 GKI_exception 65524 getbuf: out of buffers
00112110 GKI_exception(): Task State Table
00112110 GKI_exception 65524 getbuf: out of buffers
00116110 GKI_exception(): Task State Table
00116110 GKI_exception 65524 getbuf: out of buffers
00120110 GKI_exception(): Task State Table
00120110 GKI_exception 65524 getbuf: out of buffers
00124110 GKI_exception(): Task State Table
00124110 GKI_exception 65524 getbuf: out of buffers
Program control never reaches in bt/ble link management callback function. Whereas the "Out of buffers" message keeps on coming. I also tried increasing buffer count in wiced_bt_cfg_buf_pools (defined in file WICED-SDK-3.5.2\apps\snip\bluetooth\ble_hello_sensor\wiced_bt_cfg.c). But this did not help.
How can I solve this "getbuf: out of buffers" issue?
It will be very helpful if someone can provide pointers on this.
Thanks & Regards,
Pratik.
Solved! Go to Solution.
- Tags:
- gki_exception
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Depends on the profiles enabled.
But in general currently if this is BLE only then need at least 96KB of SRAM for reliable operation