- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Problem: Failed to read a packet in apps.wwd.canned_send
Make Target: wwd.canned_send-BCM943362WCD4-NoOS-NoNS-SDIO download run
and
wwd.canned_send-BCM943362WCD4-NoOS-NoNS-SPI download run
File: F:\WICED_SDK\WICED-SDK-3.1.2\Wiced-SDK\WICED\WWD\internal\wwd_thread.c
Function: int8_t wwd_thread_receive_one_packet( void )
line 183 /*@-mustfreeonly@*/ /* Failed to read a packet */
line 184 return 0;
WICED SDK: 3.1.2
PC OS: Windows XP SP3 V6223 En Version.
Modified code:
Modied WIFI parameters in
file WICED-SDK-3.1.2\Wiced-SDK\include\default_wifi_config_dct.h:
line 38 #define CLIENT_AP_SSID "999LO777VE999-WR-4"
line 39 #define CLIENT_AP_PASSPHRASE "wwwlove333666999com"
Modied WIFI parameters in
file WICED-SDK-3.1.2\Wiced-SDK\apps\wwd\canned_send\NoOS_canned_send.c
line 62 #define CLIENT_AP_SSID "999LO777VE999-WR-4"
line 63 #define CLIENT_AP_PASSPHRASE "wwwlove333666999com"
other Code from the Wiced-SDK-3.1.2-IDE-Installer.exe are NOT modified.
Could you please tell me what is wrong? I'll appreciate your help.
- Labels:
-
SDK 3.x