Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Wi-Fi Combo Forum Discussions

IVPB
Level 1
Level 1
5 replies posted 5 sign-ins First reply posted

We are evaluating the Murata Type 1GC Wi-Fi chip using WICED SDK and 43xxx_Wi-Fi project provided. 

ref: https://www.murata.com/-/media/webrenewal/products/connectivitymodule/asset/pub/rfm/data/n1-5002_typ...

Building/downloading the sample application target in step 3F (target,snip.scan-MurataType1GC), results the following error:

Creating Filesystem BCM94390x_targets.mk ...
Downloading DCT ... build/snip.scan-MurataType1GC/DCT.bin @ SFLASH_DCT_LOC=0x00008000
./tools/common/Win32/mk_wicedfs32 build/snip.scan-MurataType1GC/filesystem.bin build/snip.scan-MurataType1GC/resources/Staging/
Creating Filesystem Done
WICED/platform/MCU/BCM4390x/BCM94390x_targets.mk:394: recipe for target 'download_dct' failed
make.exe[1]: *** [download_dct] Error 1
Makefile:351: recipe for target 'main_app' failed
make: *** [main_app] Error 2

Please advise as to what may be the cause.

 

0 Likes
1 Solution
PRI
Moderator
Moderator
Moderator
100 replies posted 5 likes given 10 likes received

Hi,

You have to install the libusbK driver using Zadig. You can check out the solution of a post in the link for more info.

Thanks

View solution in original post

0 Likes
8 Replies
LeoMathews
Moderator
Moderator
Moderator
25 likes received 100 sign-ins 25 solutions authored

Hi @IVPB 

A similar issue is discussed in this link. Can you please refer to it and check if it helps? I believe this issue occurs if 2 EVKs are connected to the PC.

Thanks and Regards,
Leo

0 Likes

Hello Leo,

I do not have 2 EVK's connected when I get this failure.

Thanks,

IV

 

 

0 Likes
PRI
Moderator
Moderator
Moderator
100 replies posted 5 likes given 10 likes received

Hi,

Are you using a custom platform or a standard platform like CYW943907EVAL1F? Below are the few things that you can do to find out the cause.

1. You can add "VERBOSE=1" to your make target (snip.scan-MurataType1GC VERBOSE=1). This will give full logging of compilation & download on the console tab.

2. You can check out the "openocd_log.txt" file in the "build" directory for any errors.

Thanks

0 Likes
IVPB
Level 1
Level 1
5 replies posted 5 sign-ins First reply posted

I am using a custom platform to allow ability to change the channel setting in order  to perform a RF test.

I notice the PID and VID do not match:  

Error: no device found
Error: unable to open ftdi device with vid 04b4, pid f900, description '*', serial '*' at bus location '*'

Our FTDI cables connected via USB port are both vid: 0403 and pid: 6001

-------------------

openocd_log.txt:

Open On-Chip Debugger 0.10.0+dev-00227-g0d15c62 (2018-03-27-15:19)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
trst_and_srst separate srst_nogate trst_push_pull srst_open_drain connect_assert_srst
trst_and_srst separate srst_nogate trst_push_pull srst_open_drain connect_assert_srst
adapter speed: 100 kHz
adapter_nsrst_delay: 100
Info : auto-selecting first available session transport "jtag". To override use 'transport select <transport>'.
jtag_ntrst_delay: 100
post_init_psoc6_setup
Error: no device found
Error: unable to open ftdi device with vid 0a5c, pid 43fa, description '*', serial '*' at bus location '*'
Error: no device found
Error: unable to open ftdi device with vid 04b4, pid f900, description '*', serial '*' at bus location '*'

Verbose logs: 

Creating Filesystem BCM94390x_targets.mk ...
Downloading DCT ... build/snip.scan-MurataType1GC/DCT.bin @ SFLASH_DCT_LOC=0x00008000
./tools/common/Win32/mk_wicedfs32 build/snip.scan-MurataType1GC/filesystem.bin build/snip.scan-MurataType1GC/resources/Staging/
Creating Filesystem Done
WICED/platform/MCU/BCM4390x/BCM94390x_targets.mk:394: recipe for target 'download_dct' failed
make.exe[1]: *** [download_dct] Error 1
Makefile:351: recipe for target 'main_app' failed
make: *** [main_app] Error 2

0 Likes
IVPB
Level 1
Level 1
5 replies posted 5 sign-ins First reply posted

I've read other threads on how the Device we are trying to connect to, via USB, does not match (pid,vid).

How can we get them to match? 

Is there a specific cable/device that has to be used?

Is there any settings in the code I can change to use the device/cable we are using? 

0 Likes
PRI
Moderator
Moderator
Moderator
100 replies posted 5 likes given 10 likes received

Hi,

You're using the latest version of WICED (6.6.1) right? The verbose logs you posted don't seem right. Can you confirm you've used the following make target - "snip.scan-MurataType1GC VERBOSE=1 download run"

Ideally, you'll get logs something similar to below.

Creating Filesystem BCM94390x_targets.mk ...
"./tools/common/Win32/rm.exe" -f build/snip.gpio-CYW943907AEVAL1F/resources/Staging/app.elf
Downloading DCT ... build/snip.gpio-CYW943907AEVAL1F/DCT.bin @ SFLASH_DCT_LOC=0x00008000
.\tools\OpenOCD\Win32\openocd-all-brcm-libftdi.exe -s .\tools\OpenOCD\scripts -f ./tools/OpenOCD/CYW9WCD1EVAL1.cfg -f ./tools/OpenOCD/BCM4390x.cfg -f apps/waf/sflash_write/sflash_write.tcl -c "sflash_write_file build/snip.gpio-CYW943907AEVAL1F/DCT.bin 0x00008000 CYW943907AEVAL1F-P103-SoC.43909 0 43909" -c shutdown >> build/openocd_log.txt 2>&1
echo ./tools/common/Win32/mk_wicedfs32 build/snip.gpio-CYW943907AEVAL1F/filesystem.bin build/snip.gpio-CYW943907AEVAL1F/resources/Staging/
./tools/common/Win32/mk_wicedfs32 build/snip.gpio-CYW943907AEVAL1F/filesystem.bin build/snip.gpio-CYW943907AEVAL1F/resources/Staging/
./tools/common/Win32/mk_wicedfs32 build/snip.gpio-CYW943907AEVAL1F/filesystem.bin build/snip.gpio-CYW943907AEVAL1F/resources/Staging/
echo Creating Filesystem Done

Now, If you observe in the above logs you'll see CYW9WCD1EVAL1.cfg file ( an openocd configuration file). This cfg file is for CYW943907AEVAL1F platform and contains the vid pid values. Since yours is custom platform, i believe that you've created one cfg file with the vid pid details.

I guess that the vid pid values in your cfg file are incorrect and that's why download is failing.

Thanks

0 Likes
IVPB
Level 1
Level 1
5 replies posted 5 sign-ins First reply posted

C:\Users\IM919VO\Documents\WICED-Studio-6.6>type version.txt
WICED-SDK Version: Wiced_006.006.001.0001
b38d42ee8368ff374b13514286120afd9e788a07

IVPB_1-1676645274390.png

My device manager is not showing the libusbK and WICED USB Serial port.

 

IVPB_3-1676645432292.png

 

opedocd_log.txt

Open On-Chip Debugger 0.10.0+dev-00227-g0d15c62 (2018-03-27-15:19)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
trst_and_srst separate srst_nogate trst_push_pull srst_open_drain connect_assert_srst
trst_and_srst separate srst_nogate trst_push_pull srst_open_drain connect_assert_srst
adapter speed: 100 kHz
adapter_nsrst_delay: 100
Info : auto-selecting first available session transport "jtag". To override use 'transport select <transport>'.
jtag_ntrst_delay: 100
post_init_psoc6_setup
Error: libusb_open() failed with LIBUSB_ERROR_NOT_SUPPORTED
Error: libusb_open() failed with LIBUSB_ERROR_NOT_SUPPORTED
Error: no device found
Error: unable to open ftdi device with vid 0403, pid 6001, description '*', serial '*' at bus location '*'
Error: libusb_open() failed with LIBUSB_ERROR_NOT_SUPPORTED
Error: libusb_open() failed with LIBUSB_ERROR_NOT_SUPPORTED
Error: no device found
Error: unable to open ftdi device with vid 0403, pid 6001, description '*', serial '*' at bus location '*'

 

0 Likes
PRI
Moderator
Moderator
Moderator
100 replies posted 5 likes given 10 likes received

Hi,

You have to install the libusbK driver using Zadig. You can check out the solution of a post in the link for more info.

Thanks

0 Likes
This widget could not be displayed.