Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

In the OTA2 service, the wiced_ota2_service_get_the_update_file() erroneously returns success anytime the second call to wiced_ota2_service_wget_update() returns a non-zero error code. In the code below, if this second call fails, the return code is not saved in the result variable and when *update_result is assigned to result it gets the previous result which can only be success. See libraries/daemons/ota2_service/wiced_ota2_service.c.

wiced_result_t wiced_ota2_service_get_the_update_file(wiced_ota2_service_session_t* session, wiced_result_t* update_result)

{

    wiced_result_t  result;

    /* assume error */

    *update_result = WICED_ERROR;

    result = ota2_service_connect(session);

    if (result != WICED_SUCCESS)

    {...}

    /* get the header */

...

   /* swap the data to be correct for the platform */

...

   /* disconnect and re-connect to reset the file pointer */

    ota2_service_disconnect(session);

    result = ota2_service_connect(session);

    if ( result != WICED_SUCCESS)

    {...goto _get_file_fail;}

    /* get the OTA2 file */

/*if ( wiced_ota2_service_wget_update(session, NULL, 0) != WICED_SUCCESS) Replaced with the following 2 lines*/

    result = wiced_ota2_service_wget_update(session, NULL, 0);

    if ( result != WICED_SUCCESS)

    {

        OTA2_LIB_PRINT(session, OTA2_LOG_ERROR, ("wiced_ota2_service_get_the_update() wiced_ota2_service_wget_update(file) failed!\r\n"));

        wiced_ota2_service_make_error_callback(session, OTA2_SERVICE_UPDATE_ERROR );

        session->download_failures++;

        *update_result = result;

        goto _get_file_connected_fail;

    }

...

   /* we succeeded in getting the file here */

    *update_result = WICED_SUCCESS;

_get_file_connected_fail:

    ota2_service_disconnect(session);

_get_file_fail:

    return result;

}

1 Solution
PriyaM_16
Moderator
Moderator
Moderator
250 replies posted 100 replies posted 50 replies posted

Hello,

Thanks for pointing out the error. The change is incorporated in WICED SDK.

View solution in original post

0 Likes
1 Reply
PriyaM_16
Moderator
Moderator
Moderator
250 replies posted 100 replies posted 50 replies posted

Hello,

Thanks for pointing out the error. The change is incorporated in WICED SDK.

0 Likes