Driver support required for BCM9WCDPLUS1_2.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

After plugging BCM9WCDPLUS1_2. eval board  to my laptop, two usb Serial Ports are automatically detected and installed.

WICED USB JTAG port is not installed as it happens for a WICED-Wifi board.

I am trying to flash smart ip_bridge software on to this BCM9WCDPLUS1_2 eval board and I get error as ..

"**** OpenOCD failed - ensure you have installed the driver from the drivers directory, and that the debugger is not running ****

i assume the JTAG drivers are not installed for this board or that is not detected at all.

Please let me know the steps to go further

Regards

Yasin

0 Likes
1 Reply
SeyhanA_31
Employee
Employee
250 replies posted 100 replies posted 50 replies posted

Hi,

Drivers for the USB to JTAG and serial ports are located at .../tools/drivers directory of the SDK. Uninstall and install the drivers for USB-JTAG device which comes with the Wiced evaluation board. You can refer to quick starter guide QSG for detailed info.

Seyhan

0 Likes