Does Infineon have plans to support existing radio modules hosted with ST or Microchip MCUs in feature upgrades for WICED orModusToolbox?

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
GrCa_1363456
Level 6
Level 6
50 likes received Beta tester First comment on KBA

For customers starting a new design with a module paired with an ST or Microchip MCU, what assurance do they have that they’ll be supported with necessary firmware features as support for WICED migrates over to ModusToolbox?

Does Infineon have plans to support existing Cypress based radio modules hosted with ST and Microchip microcontrollers in ModusToolbox?

If support in ModusToolbox for modules hosted by an attached microcontroller is up to the Module Partner, is there a process to support those module partners that I can reference when asking each of them of their plans to add ModusToolbox support for existing modules?

Some of the modules hosted by ST and Microchip fall into this category include:

Azurewave AW-CU307 based on CYW43362 with STM32411

Azurewave AW-CU289 based on CYW43438 with STM32F412

Inventek ISM43362-M3G-L44-E based on CYW43362 with STM32F205

Inventek ISM4343-WBM-L151 based on CYW4343W with STM32F411

Lantronix XPCW1002100B based on CYW43362 with STM32F205

Lantronix PW205010001B based on CYW4339 with AT91SAM9G25

Laird Sterling EWB based on CYW4343W with STM32F412

Murata Type 1HD (LBWA1ZZ1HD-004) based on CYW43438 with STM32F412

Murata Type 1LD (LBEE5PA1LD-005) based on CYW43438 with STM32F412

ModusToolbox currently supports several of the above radios including:

- CYW43012

- CYW4343W

- CYW43438

It would also be helpful to know how Infineon plans to support two radios in the above modules not currently showing up in ModusToolbox:

- CYW43362

- CYW4339

Greg

For customers starting a new design with a module paired with an ST or Microchip MCU, what assurance do they have that they’ll be supported with necessary firmware features as support for WICED migrates over to ModusToolbox?

Does Infineon have plans to support existing Cypress based radio modules hosted with ST microcontrollers in ModusToolbox?

If support in ModusToolbox for modules hosted by an attached microcontroller is up to the Module Partner, is there a process to support those module partners that I can reference when asking each of them of their plans to add ModusToolbox support for existing modules?

Some of the modules hosted by ST and Microchip fall into this category include:

·       Azurewave AW-CU307 based on CYW43362 with STM32411

·       Azurewave AW-CU289 based on CYW43438 with STM32F412

·       Inventek ISM43362-M3G-L44-E based on CYW43362 with STM32F205

·       Inventek ISM4343-WBM-L151 based on CYW4343W with STM32F411

·       Lantronix XPCW1002100B based on CYW43362 with STM32F205

·       Lantronix PW205010001B based on CYW4339 with AT91SAM9G25

·       Laird Sterling EWB based on CYW4343W with STM32F412

·       Murata Type 1HD (LBWA1ZZ1HD-004) based on CYW43438 with STM32F412

·       Murata Type 1LD (LBEE5PA1LD-005) based on CYW43438 with STM32F412

ModusToolbox currently supports several of the above radios including:

-          CYW43012

-          CYW4343W

-          CYW43438

It would also be helpful to know how Infineon plans to support two radios in the above modules not currently showing up in ModusToolbox:

-          CYW43362

-          CYW4339

For customers starting a new design with a module paired with an ST or Microchip MCU, what assurance do they have that they’ll be supported with necessary firmware features as support for WICED migrates over to ModusToolbox?
Does Infineon have plans to support existing Cypress based radio modules hosted with ST microcontrollers in ModusToolbox?
If support in ModusToolbox for modules hosted by an attached microcontroller is up to the Module Partner, is there a process to support those module partners that I can reference when asking each of them of their plans to add ModusToolbox support for existing modules?
Some of the modules hosted by ST and Microchip fall into this category include: Azurewave AW-CU307 based on CYW43362 with STM32411 Azurewave AW-CU289 based on CYW43438 with STM32F412 Inventek ISM43362-M3G-L44-E based on CYW43362 with STM32F205 Inventek ISM4343-WBM-L151 based on CYW4343W with STM32F411 Lantronix XPCW1002100B based on CYW43362 with STM32F205 Lantronix PW205010001B based on CYW4339 with AT91SAM9G25 Laird Sterling EWB based on CYW4343W with STM32F412 Murata Type 1HD (LBWA1ZZ1HD-004) based on CYW43438 with STM32F412 Murata Type 1LD (LBEE5PA1LD-005) based on CYW43438 with STM32F412
ModusToolbox currently supports several of the above radios including:- CYW43012- CYW4343W- CYW43438
It would also be helpful to know how Infineon plans to support two radios in the above modules not currently showing up in ModusToolbox:- CYW43362- CYW4339

dddyyy

0 Likes
1 Solution
MichaelF_56
Moderator
Moderator
Moderator
250 sign-ins 25 comments on blog 10 comments on blog

Greg,

Per our email dialog, I will call you next week and provide a detailed strategy discussion on our various partner based RTOS/MCU combinations.

Mike

MuraliR_36​  MarkS_11

View solution in original post

0 Likes
1 Reply
MichaelF_56
Moderator
Moderator
Moderator
250 sign-ins 25 comments on blog 10 comments on blog

Greg,

Per our email dialog, I will call you next week and provide a detailed strategy discussion on our various partner based RTOS/MCU combinations.

Mike

MuraliR_36​  MarkS_11

0 Likes