- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I added spi master code in Wiced scan example code with CYW943012EVB(STM32L4A6+CYW43438) ,
and connect it to CY8CPROTO-062-4343W to control led via spi interface.
It seems spi master not work in CYW943012EVB, does Cypress have any spi master example code?
Code:
SPI_HandleTypeDef SPI1_Handler;
void SPI1_Init(void)
{
SPI1_Handler.Instance=SPI1;
SPI1_Handler.Init.Mode=SPI_MODE_MASTER;
SPI1_Handler.Init.Direction=SPI_DIRECTION_2LINES;
SPI1_Handler.Init.DataSize=SPI_DATASIZE_8BIT;
SPI1_Handler.Init.CLKPolarity=SPI_POLARITY_HIGH;
SPI1_Handler.Init.CLKPhase=SPI_PHASE_2EDGE;
SPI1_Handler.Init.NSS=SPI_NSS_SOFT;
SPI1_Handler.Init.BaudRatePrescaler=SPI_BAUDRATEPRESCALER_16;
SPI1_Handler.Init.FirstBit=SPI_FIRSTBIT_MSB;
SPI1_Handler.Init.TIMode=SPI_TIMODE_DISABLE;
SPI1_Handler.Init.CRCCalculation=SPI_CRCCALCULATION_DISABLE;
HAL_SPI_Init(&SPI1_Handler);
}
void HAL_SPI_MspInit(SPI_HandleTypeDef *hspi)
{
GPIO_InitTypeDef GPIO_Initure;
if(hspi->Instance==SPI1)
{
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_SPI1_CLK_ENABLE();
GPIO_Initure.Pin=GPIO_PIN_1|GPIO_PIN_6|GPIO_PIN_7;
GPIO_Initure.Mode=GPIO_MODE_AF_PP;
GPIO_Initure.Pull=GPIO_PULLUP;
GPIO_Initure.Speed=GPIO_SPEED_HIGH;
GPIO_Initure.Alternate=GPIO_AF5_SPI1;
HAL_GPIO_Init(GPIOA,&GPIO_Initure);
}
}
void application_start( )
{
uint8_t txData=0x00;
wiced_init( );
SPI1_Init();
HAL_SPI_Init(&SPI1_Handler);
while(1)
{
wiced_time_t scan_start_time;
wiced_time_t scan_end_time;
app_scan_data_t scan_data;
/* Initialize the semaphore that will tell us when the scan is complete */
wiced_rtos_init_semaphore(&scan_data.semaphore);
scan_data.result_count = 0;
WPRINT_APP_INFO( ( "Waiting for scan results...\n" ) );
WPRINT_APP_INFO( (" # Type BSSID RSSI Rate Chan Security SSID CCode Flag\n" ) );
WPRINT_APP_INFO( ("------------------------------------------------------------------------------------------------------------------\n" ) );
/* Start the scan */
wiced_time_get_time(&scan_start_time);
wiced_wifi_scan_networks(scan_result_handler, &scan_data );
/* Wait until scan is complete */
wiced_rtos_get_semaphore(&scan_data.semaphore, WICED_WAIT_FOREVER);
wiced_time_get_time(&scan_end_time);
WPRINT_APP_INFO( ("\nScan complete in %lu milliseconds\n", (unsigned long )(scan_end_time - scan_start_time) ) );
/* Clean up */
wiced_rtos_deinit_semaphore(&scan_data.semaphore);
/* Issuing next scan after some delay (optional) */
txData = 0;
WPRINT_APP_INFO( ( "txData=%d\n", txData ) );
HAL_SPI_Transmit(&SPI1_Handler, &txData, 1, 1000);
wiced_rtos_delay_milliseconds(DELAY_BETWEEN_SCANS);
txData = 1;
WPRINT_APP_INFO( ( "txData=%d\n", txData ) );
HAL_SPI_Transmit(&SPI1_Handler, &txData, 1, 1000);
}
}
- Tags:
- STM32L4A6 spi master
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello:
CYW943012EVB(STM32L4A6+CYW43012), is this right? Actually, You are using SPI of STM32L4A6 to connect with the SPI of CY8CPROTO-062-4343W , Psoc6, is this right ?
So Psoc6 is the slave side , How did you confirm SPI master not working in STM side ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Yes, I'm using CYW943012EVB_04.
SPI master : PSoC6(CY8CPROTO-062-4343W)
SPI slave: STM32L4A6(CYW943012EVB_04)
Because I have no scope at my hand, I use digital multimeter measure SPI clock.
While spi enabling , I can see voltage jump from 0~1.7V on PSoC6, but STM32L4A6 spi clock voltage always = 0V.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello:
I can't find accurate memo for STM32L4XX SPI usage, but you can have a check on below address:
WICED/platform/MCU/STM32L4xx/peripherals/libraries/Drivers/STM32L4xx_HAL_Driver/src/stm32l4xx_II_spi.c , you can get api from this c file, and try to find the usage from instructions and the code.