Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Anonymous
Not applicable

error.png

We are doing power test.

I am using the while function to send http every 5 seconds.

wiced_rtos_delay_milliseconds (5000);

Is it correct use?

Do you have a sleep mode?

Are there good features to reduce power consumption?

In the case of Bluetooth, there was a sleep mode. Is there a sleep mode even in the case of Wi-Fi?

Please tell us.

I'm sorry I did not speak English.

Thank you.

1 Solution
GauravS_31
Moderator
Moderator
Moderator
250 solutions authored 250 sign-ins First comment on KBA

You can refer to powersave app note available in directory /43xxx_Wi-Fi/doc/WICED-Powersave-App-Note.pdf. Broadly speaking, there are two types of powersave: Wi-Fi 802.11 powersave and MCU powersave. You can refer to the app note for more information. As long as sufficient time delay is provided for HTTP response, it is okay to use the while loop.

View solution in original post

2 Replies
GauravS_31
Moderator
Moderator
Moderator
250 solutions authored 250 sign-ins First comment on KBA

You can refer to powersave app note available in directory /43xxx_Wi-Fi/doc/WICED-Powersave-App-Note.pdf. Broadly speaking, there are two types of powersave: Wi-Fi 802.11 powersave and MCU powersave. You can refer to the app note for more information. As long as sufficient time delay is provided for HTTP response, it is okay to use the while loop.

A better approach would be to use wiced_rtos_get_semaphore(&sem,WICED_WAIT_FOREVER); instead of delay and use wiced_rtos_set_semaphore(&sem); in the HTTP response callback function.