- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I am using CYW54907 dev board, WICED SDK 6.6. My board is placed in a mix 2.4GHz, 5GHz network, 2 network has different SSID.
Normally, I can connect to 2.4GHz network and 5GHz network well. But sometimes I cant connect 2.4GHz network or even if I connect the network successfully, I cant get the ip address. I did use a phone hotspot and place the hotspot near my board, but it still can't connect. The issue lasts for 1-2 days.
I don't store ssid and password on default_wifi_config_dct.h or on dct field, I join network using wiced_join_ap_specific(). Strangely enough, if I load scan example, put my network info in default_wifi_config_dtc.h, let it autoconnect via wiced_init(), and constantly press reset button, it can recover. I don't see this case with 5GHz network.
What is the problem with my board and how can i troubleshoot it? I had some fellows who connect to 2.4GHz smoothly, but their environment doesn't have 5GHz network, so I wonder if it's because of my dev board hardware or the mixed 2.4GHz and 5GHz network has some unwanted effects on joining network.
Thanks
Solved! Go to Solution.
- Labels:
-
WICED Studio Wi-Fi Combo
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I tried your code example and tried to connect to a 2.4GHz network i.e. my phone's hotspot. I was able to connect to the network successfully. I tried resetting a few times, sometimes the join failed but on the next reset the join passes. I can change the band of my phone's hotspot to 5 GHz as well. Basically, mine is also a mixed environment.
So, the issue is not reproducible in my setup. Ideally, mix environment shouldn't cause such issues. I will suggest trying with other APs of mixed environments and seeing if the issue is reproducible in that case.
Thanks
Aditi
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Can you provide the code example that you're using in your case setup?
Thanks
Aditi
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Here is the code example, written in cpp. Hope it help. It needs to connect 4-5 days continuously before can connect to 2.4GHz network in 1-2 days.
#include <internal/wiced_internal_api.h>
#include "wiced.h"
uint32_t connect_to_wifi(wiced_ap_info_t* wicedApInfo, uint8_t passwordLen, const char* password) {
wiced_result_t result;
if (wicedApInfo->security == WICED_SECURITY_OPEN) {
result = wiced_join_ap_specific(wicedApInfo, 0, 0);
} else {
result = wiced_join_ap_specific(wicedApInfo, passwordLen, password);
}
WPRINT_APP_INFO(("Connect to SSID=%s err=%d\n\n", wicedApInfo->SSID.value, result));
if (result == WICED_SUCCESS) {
result = wiced_ip_up(WICED_STA_INTERFACE, WICED_USE_EXTERNAL_DHCP_SERVER, NULL);
}
return result;
}
void application_start(void) {
wiced_init();
wiced_ap_info wicedApInfo;
memset(&wicedApInfo, 0, sizeof(wicedApInfo));
const char* ssid = "SSID 2.4G";
const char* password = "12345678";
wicedApInfo.SSID.length = strlen(ssid);
memcpy(wicedApInfo.SSID.value, ssid, strlen(ssid));
wicedApInfo.bss_type = WICED_BSS_TYPE_INFRASTRUCTURE;
wicedApInfo.security = WICED_SECURITY_WPA2_MIXED_PSK;
auto ret = connect_to_wifi(&wicedApInfo, strlen(password), password);
WPRINT_APP_INFO(("connect_to_wifi err=%d\n\n", ret));
}
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I tried your code example and tried to connect to a 2.4GHz network i.e. my phone's hotspot. I was able to connect to the network successfully. I tried resetting a few times, sometimes the join failed but on the next reset the join passes. I can change the band of my phone's hotspot to 5 GHz as well. Basically, mine is also a mixed environment.
So, the issue is not reproducible in my setup. Ideally, mix environment shouldn't cause such issues. I will suggest trying with other APs of mixed environments and seeing if the issue is reproducible in that case.
Thanks
Aditi