Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Anonymous
Not applicable

Hello

I need the datasheet of BCM943362WCD4_EVB.

which is a evboardfor Wi-fi.

I need its clock frequenecy, SPI speed etc.

1 Solution
Anonymous
Not applicable

It uses STM32F205. CPU clock frequency is 120MHz.

SPI1 supports up to 30MHz and SPI2 and SPI3 support up to 15MHz.

View solution in original post

1 Reply
Anonymous
Not applicable

It uses STM32F205. CPU clock frequency is 120MHz.

SPI1 supports up to 30MHz and SPI2 and SPI3 support up to 15MHz.