With the newly released SDK 3.1, it appears that the old DCT read/write functions have been deprecated. However, I'm seeing issues with the new functions when writing to the application section. I'm not able to read a previously written value in the application section.
wiced_dct_read_lock( (void**) &p_test, WICED_FALSE, DCT_APP_SECTION, 0, sizeof(some_struct_t)) );
p_test->test = 2;
wiced_dct_write( (const void*) p_test, DCT_APP_SECTION, 0, sizeof(some_struct_t) );
wiced_dct_read_unlock( p_test, WICED_FALSE );
wiced_dct_read_lock( (void**) &p_test, WICED_FALSE, DCT_APP_SECTION, 0, sizeof(some_struct_t) );
WPRINT_APP_INFO(("Rereading test ID after write=%ld\r\n", (long int)p_test->test));
wiced_dct_read_unlock( p_test, WICED_FALSE );
I see "Rereading test ID after write=-1" on the UART.
Can someone from the WICED team please see if there is an issue with the above code and if it should have been working.
Thanks.
Solved! Go to Solution.
Hi,
There has been some changes for storing and retrieving DCT data from SDK-2.4.1 to SDK-3.1.0.
Please check the header file or documentation for the APIs for more information.
Here is the functions parameter as follows:
/** Reads the DCT and returns a pointer to the DCT data
*
* The operation of this function depends on whether the DCT is located in
* external or internal flash memory.
* If ptr_is_writable is set to false and the DCT is located in internal flash,
* then a direct pointer to the flash memory will be returned.
* Otherwise memory will be allocated and the DCT data will be copied into it.
*
* @note : this function must be used in pairs with wiced_dct_read_unlock to
* ensure that any allocated memory is freed.
*
* @param info_ptr [out] : a pointer to the pointer that will be filled on return
* @param ptr_is_writable [in] : if true then then the returned pointer will be in RAM
* allowing it to be modified. e.g. before being written
* @param section [in] : the section of the DCT which should be read
* @param offset [in] : the offset in bytes within the section
* @param size [in] : the length of data that should be read
*
* @return Wiced Result
*/
extern wiced_result_t wiced_dct_read_lock( void** info_ptr, wiced_bool_t ptr_is_writable, dct_section_t section, uint32_t offset, uint32_t size );
-Seyhan
Making the second parameter of wiced_dct_read_lock and wiced_dct_read_unlock functions from FALSE to TRUE gets things working, Still not clear on the reason.
Thanks,
Hi,
There has been some changes for storing and retrieving DCT data from SDK-2.4.1 to SDK-3.1.0.
Please check the header file or documentation for the APIs for more information.
Here is the functions parameter as follows:
/** Reads the DCT and returns a pointer to the DCT data
*
* The operation of this function depends on whether the DCT is located in
* external or internal flash memory.
* If ptr_is_writable is set to false and the DCT is located in internal flash,
* then a direct pointer to the flash memory will be returned.
* Otherwise memory will be allocated and the DCT data will be copied into it.
*
* @note : this function must be used in pairs with wiced_dct_read_unlock to
* ensure that any allocated memory is freed.
*
* @param info_ptr [out] : a pointer to the pointer that will be filled on return
* @param ptr_is_writable [in] : if true then then the returned pointer will be in RAM
* allowing it to be modified. e.g. before being written
* @param section [in] : the section of the DCT which should be read
* @param offset [in] : the offset in bytes within the section
* @param size [in] : the length of data that should be read
*
* @return Wiced Result
*/
extern wiced_result_t wiced_dct_read_lock( void** info_ptr, wiced_bool_t ptr_is_writable, dct_section_t section, uint32_t offset, uint32_t size );
-Seyhan
Thanks Seyhan. I agree, the parameter section does explain it.
Regards.