Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

When attempting to compile the OpenOCD from it's source directory @

<root>/toosl/OpenOCD/source/...

I found that it wouldn't compile due to incompatibility with clang 3.6.

The  error was :

../../../../src/flash/nor/sim3x.c:867:20: error: address of array

'sim3x_info->device_package' will always evaluate to 'true' .

Googling it, it seems that this issue was already resolved, and there is a patch for it.

In ordet to apply the patch into the existing scripts, one would need to:

1. download the attached file and place in under <root>/toosl/OpenOCD/source/patches

2. update the just_oocd.sh and add the patch file name as follows:

git am ../patches/0027-TCL-Delete-files-with-unicode-names-that-MinGW-can-t.patch

git am ../patches/0028-Fix-up-RTOS-implementation-for-FreeRTOS-ThreadX.patch

git am ../patches/0029-Cortex-A-Revert-changes-which-break-the-sflash-write.patch

git am ../patches/169db31a.patch

cd ..

After that, the OpenOCD should be built and run just fine... assuming you already had the Xcode and Xcode command line tools installed. ( OS X only )

I haven't seen that on the SDK build notes, but it's an additional prerequisite that is clearly needed.

Tsachi

0 Replies