- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I have three CY8CKIT-062-WiFi-BT. Out of the box all kits are able to be programmed with wiced examples.
I have done the following with two of the three kits:
I used fw-loader to upgrade to KitProg3 so I could try modus.
I used fw-loader to downgrade to KitProg2 so I could go back to wiced.
Since I went back to KitProg2 I have not been able to program with wiced. See error below.
According to the documentation I should be able to use fw-loader to switch between KitProg2 and KitProg3. This does not work for me.
I have tried every possible led configuration
The board with original kitprog2 works fine.
The two boards that went to kitprog3 and then back to kitprog2 do not work.
Thoughts?
Error:
Downloading Bootloader ...
Building apps lookup table
"**** OpenOCD failed - ensure you have installed the driver from the drivers directory, and that the debugger is not running **** In Linux this may be due to USB access permissions. In a virtual machine it may be due to USB passthrough settings. Check in the task list that another OpenOCD process is not running. Check that you have the correct target and JTAG device plugged in. ****"
Downloading DCT ...
"**** OpenOCD failed - ensure you have installed the driver from the drivers directory, and that the debugger is not running **** In Linux this may be due to USB access permissions. In a virtual machine it may be due to USB passthrough settings. Check in the task list that another OpenOCD process is not running. Check that you have the correct target and JTAG device plugged in. ****"
Downloading resources filesystem ... build/ww101.02.04_button-CY8CKIT_062/filesystem.bin at sector 1 size 104...
tools/makefiles/wiced_apps.mk:335: recipe for target 'FILESYSTEM_IMAGE_DOWNLOAD' failed
make.exe[1]: *** [FILESYSTEM_IMAGE_DOWNLOAD] Error 1
make: *** [main_app] Error 2
Makefile:351: recipe for target 'main_app' failed
Solved! Go to Solution.
- Labels:
-
ispn:39620:1:0
-
l1:314:1:0
-
WICEDStudio
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
OpenOCD Failed, CY8CKIT-WiFi-BT Pioneer Kit
You may want to follow this thread... I added some of my trials and tribulations...
(note: I am using Windows 7 Pro so it may differ but should be very similar under Windows 10)
In Windows 10; click "search" icon, in search type "device installation settings"
click "no"; save
go to device manager select the port, make sure the device is plugged in and in correct mode... or at least the Programmer states it is in dap mode, the devkit may have led2 and led4 lit and steady, that is the mode I performed the steps in, afterwards, I got the correct indication from the dev kit of led4 lit and no other led's were lit. That is correct mode to program with WICED...
Right click and select update driver and select browse my computer
Then let me pick, untick "show compatible hardware"; select Cypress; select Wiced Peripheral UART
Select "have disk"
Navigate to C:(where ever you have WICED installed..)\WICED-Studio-6.4\Drivers\Windows\wiced_uart
Select wicedport.inf
Let that install...
Now it may Let you know "installing new device" or not, it not unplug DevKit and plug it back in. Make SURE that you did these steps!!!:
In Windows 10; click "search" icon, in search type "device installation settings"; click "no"; save
Anyway you will see the "installing new device" then, go to device manager, your goal is to see the kitProg2 device under Portable Devices"
Here is what I think happened, you had it installed properly, when you powered off and back on Windows 10 in its infinite wisdom installed the driver that "it" thought was best. I read an article about that, I've read so many articles, I could not re-reference it... But they were only speaking about Windows 7 which, I've never had as much issues with, as I have with Windows 10!!! which "they" shoved down our throats imho... Oh... uh I guess that is not nice
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Other things I have tried:
Plugged both boards into computer at the same time and compared properties of KitProg2 via windows device manager. The only difference is install date. All other pertinent info is the same (version, etc).
On my untouched board, the one that still works, led4 (power) is the only led that is lit. When the problem boards are in this same configuration they produce the error.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
The plot thickens. See psoc programmer image below. Under Port Selection there are two entries. The first one is for the board that works. The second one is for the board that does not work.
The following warning pops up whenever I plug any board in while psoc programmer is running. The update firmware button is always disabled.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Just to clarify, I am not using psoc programmer to program. Just to help debug this issue.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
On the CY8CKIT062-WIFI BT board, there is a mode select switch (S3). Press the SW3 button on your board. After this, LED2 and LED4 will be lit. You will be able to program your board in WICED since the kit is now in HID Mode.
Thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thanks for your response AditiB_81. I forgot to mention that previously I tried every possible configuration that SW3 provides with no luck. The following screenshot illustrates the result of trying to download with LED2 and LED4 lit.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
You can use fw-loader(Firmware Loader) from Modus Toolbox 2.1 release.You can display the list of your connected devices and can get the information of the mode of your connected device using this fw-loader by using the command fw-loader --device-list. Could you please check this command and attach the screenshot of the same?
Thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Here are both boards with LEDs 2 and 4 lit:
Neither board can be programmed in this configuration. Both return this error: "**** OpenOCD failed..."
This is the same error returned when no boards are plugged in. This has to be an important clue.
Here are both boards with only LED4 lit:
The good board (1719...) can be programmed just fine.
The bad board (1C21...) returns "**** OpenOCD failed..." as if the board is not recognised or not plugged in at all.
See image I posted on April 22, 2020 7:58 AM for complete error.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi BeCo_289361,
First of all, I tried programming a WICED Project with KitProg3 HID mode (LED4 will be lit and LED2 will function as a breathing LED) and it works fine. To toggle to HID mode without pressing SW3, in the FW-loader, use the command fw-loader --mode kp3-hid.
Second, I could not see any issues with toggling between KitProg 3 and KitProg 2. KitProg2 HID mode appears as a mass storage device (like a USB drive - KitProg2 (D:)). If you view the Device Manager by 'Devices by connection', the KitProg 2 HID appears like the image shown below.
As AditiB_81 mentioned, WICED projects can be programmed only in HID mode (Correction: Only LED4 will be lit)
-73.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
8. Re: Cannot program WiFi BT Pioneer Kit after switching to kitprog3 and then back to kitprog2
Hi SanjeevG_16
KitProg3 results:
When using kitProg3 I can't get only LED4 to be lit. I have tried with SW3 and fw-loader. The modes do appear to change according to "fw-loader --device-list", however, LED4 is never the only LED lit. When downloading with kitProg3 the error is always the same as illustrated in my Apr 22, 2020 7:58 AM post.
KitProg2 results:
Only LED 4 is lit. Still get same error. Our device managers are very different. Am I missing a driver?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
The device manager when using my good board is exactly the same as when using bad board.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
My setup:
Lenovo Y70
win 10
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi BeCo_289361,
For KP3, the HID mode is indicated by breathing LED2 (at 1Hz). For KP2 HID, LED2 will not be lit.
I can see the drivers remain the same. Thanks for confirmation.
Further debugging:
So, in KP3, there are three modes present - CMSIS-DAP BULK, CMSIS-DAP HID and an other mode called DAP-LINK. the DAP-LINK is a custom application downloaded into the KitProg.
In KP2, only two modes present in which one of them is in HID. But when you try to transition from KP3 to KP2, the custom application DAP-LINK is unaffected. If you have downgraded your kit to KP2, you can switch to DAP-LINK by pressing SW4.
Now, I want you to do two things,
First, when in KP3 - Try the command fw-loader --mode kp3-daplink on the command line. Then try downloading the application.
Second, when in KP2, Press the switch SW4. Now, try downloading the FW and let me know if any of the two steps work.
-73.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
kitProg3:
fw-loader --mode kp3-daplink
kitProg2:
press sw4 once = led 4 lit, led2 breathing.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
You can try programming your WICED application with Kitprog2 CMSIS-DAP HID mode. I downgraded to Kitprog2 from Kitprog3 using fw-loader and I can successfully build the code. You can try the following steps to build your application successfully.
Following your sequence of steps:
--> Upgraded to Kitprog3 using fw-loader for MODUS applications.
-->Downgraded to kitprog2 using fw-loader for WICED applications.
--> Change to Kitprog2 CMSIS-DAP HID mode for building WICED applications by pressing SW3. After this check for the mode through fw-loader using the command fw-loader --device-list. Only LED4 will be lit on the board.
--> Build your application in WICED. I am attaching the build log and openocd.txt files.
Thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
AditiB_81,
After studying your output I noticed my fw-loader version was different. I upgraded to version 2.3.0.568 which is the same as yours.
I switched to kp3 and back to kp2. Pressed SW3 until LED4 was the only one lit.
I then tried to download and got the same results as before. See attached log. I deleted the log so what is in the log is from a single try.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi BeCo_289361,
Sorry about the time taken to find the solution. I still am figuring out what is the issue. Can you answer this question: When you try to switch to KitProg2 HID or KitProg3 DAPLINK, do you see the kit as a mass storage device (seperate drive eg:(D:)) on the PC?
-73
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
SanjeevG_16,
Simple answer is yes.
Details:
kp2 -- LED4 is the only one lit.
kp3 -- LED2 is strobing. LED4 is on solid.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I have gone through your openocd log file and I see that it throws the error of "Target not examined, reset NOT asserted!" . Could you please share three .cfg files of WICED? These are:
-->psoc62_gdb_jtag.cfg
-->psoc62-flash-app.cfg
-->psoc62.cfg
Location in WICED: ./tools/OpenOCD
Thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I did a fresh install to see if that would magically fix this. It didn't. The problem is still exactly the same.
Attached are the files you asked for.
I now own five of the kits. Two are in this unusable state. The interesting thing is that the two that don't work are in the hands of two different people. I have one. My employee who lives in another state has the other. We both ended up in this mess on our own without consulting the other.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
One more thing. When I did the reinstall I came across this:
Note 1: The config.eml file needed for the installation process (must reside in same physical folder as installer during install process) is included as an attachment at the bottom of this page. The config.eml file was not included in the same .zip file as the installer . (as done with previous SDK releases).
There was no config.eml file at the bottom of the page. And there was a config.eml file with the *.exe installer. I proceeded with the install.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi, I have the similar problem.
And in my openocd_log
Open On-Chip Debugger 0.10.0+dev-00227-g0d15c62 (2018-03-27-15:19)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : auto-selecting first available session transport "swd". To override use 'transport select <transport>'.
adapter speed: 1000 kHz
cortex_m reset_config sysresetreq
cortex_m reset_config vectreset
post_init_psoc6_setup
Error: unable to open CMSIS-DAP device 0x4b4:0xf148
But in PSoC Programmer, it is CMSIS-DAP
May I know the demo you run to get the openocd_log and buildlog?
Thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Please create a new thread for your query. We'll be more than happy to help you there.
Thanks
Aditi
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Try this...
https://www.cypress.com/products/psoc-programming-solutions
Make sure you have downloaded latest PSoC Programmer 3.28.7 if you haven't already
Reflash with --update-kp2
Then start your PSoC Programmer 3.28.7
When you get
Click "OK" then just click "Load from device" that should put you back where you need to be
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I did as you suggested. After pressing "Load from device" this is what I get:
Result of Make Target:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Notice that my versions are much newer than yours. Just wondering, do you now get just led4 lit instead of led4 lit and led2 breathing?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
ModusToolbox ver. 2.1.0
fw-loader ver.2.3.0.568
Windows Version? if its Windows 7 I know exactly what your issue is!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Even if your windows version is not Windows 7 you may still have the wrong driver installed. I was only able to get WICED working by switching back to kitprog2 and installing the WICED-uart driver that comes with WICED 6.4.0.61.
Did you follow the instuctions about setting up C:\TEMP etc, etc?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
LED4 only.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Me:
win 10
modus 2.1.0
wided 6.4.0.61 - have installed several times
fw-loader 2.3.0.568
Yes I did set up C:\TEMP etc, etc.
How do I install WICED-uart driver that comes with WICED 6.4.0.61?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
OpenOCD Failed, CY8CKIT-WiFi-BT Pioneer Kit
You may want to follow this thread... I added some of my trials and tribulations...
(note: I am using Windows 7 Pro so it may differ but should be very similar under Windows 10)
In Windows 10; click "search" icon, in search type "device installation settings"
click "no"; save
go to device manager select the port, make sure the device is plugged in and in correct mode... or at least the Programmer states it is in dap mode, the devkit may have led2 and led4 lit and steady, that is the mode I performed the steps in, afterwards, I got the correct indication from the dev kit of led4 lit and no other led's were lit. That is correct mode to program with WICED...
Right click and select update driver and select browse my computer
Then let me pick, untick "show compatible hardware"; select Cypress; select Wiced Peripheral UART
Select "have disk"
Navigate to C:(where ever you have WICED installed..)\WICED-Studio-6.4\Drivers\Windows\wiced_uart
Select wicedport.inf
Let that install...
Now it may Let you know "installing new device" or not, it not unplug DevKit and plug it back in. Make SURE that you did these steps!!!:
In Windows 10; click "search" icon, in search type "device installation settings"; click "no"; save
Anyway you will see the "installing new device" then, go to device manager, your goal is to see the kitProg2 device under Portable Devices"
Here is what I think happened, you had it installed properly, when you powered off and back on Windows 10 in its infinite wisdom installed the driver that "it" thought was best. I read an article about that, I've read so many articles, I could not re-reference it... But they were only speaking about Windows 7 which, I've never had as much issues with, as I have with Windows 10!!! which "they" shoved down our throats imho... Oh... uh I guess that is not nice
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hey BeCo_289361,
This issue has not been marked answered... If it was resolved, then please let me know what it was... Thanks!
If not, I was looking over this again, some statements you made got my attention...
First:
You stated:
"There was not config.eml file at the bottom of the page. And there was a config.eml file with the *.exe installer. I proceeded with the install"
Second:
You did the install as you point out, BUT, I believe it was done with a previous SDK release based on previous statement above.
Please reference WICED-Studio 6.4.0 Installer (Windows)
Scroll all the way to bottom, click and download: config.eml, README_WINDOWS.txt.zip, and WICED-Studio-6.4.0.61-IDE-Installer.exe.zip
The WICED-Studio-6.4.0.61-IDE-Installer.exe.zip will NOT contain config.eml, this is the correct (latest) version...
As pointed out in the link I provided ( WICED-Studio 6.4.0 Installer (Windows) 😞 I placed the downloaded config.eml and unzipped WICED installer.exe in C:\TEMP
Note: the ProxyName.ini was generated during install "5/19/2020 2:40 PM"
As you will see when you click on the link I provided ( WICED-Studio 6.4.0 Installer (Windows) ), Michael_56 points out the following:
Note 2:
There is a known installer issue which occurs when white space is included in the path to the temp folder.
To overcome this issue, do the following:
- Create a folder: c:\temp
- Open Windows Control Panel->System -> Advanced System Setting -> Environment Variables
- Edit TEMP and TMP path to use c:\temp
-->In my case, C:\TEMP already existed. So all I did was to make sure it was under System Variable, in my case it was.
If that is not the case with you, then make sure System Variable TEMP value is: %SystemRoot%\TEMP
I did not change TMP to use C:\TEMP
Then double-click on WICED-Studio-6.4.0.61-IDE-Installer.exe in C:\TEMP to install...
I recommend the following in the order stated:
- Use Programmer to reflash to KitProg2 with --update-kp2
- Reinstall your WICED Driver: \WICED-Studio-6.4\Drivers\Windows\wiced_uart\wicedport.inf
- Rebuild and "hopefully" finally... flash your application!
See if this helps...