Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

chch_2120956
Level 3
Level 3
First like received First like given

I compile the projector (wwd.canned_send-BCM943362WCD2-NoOS-NoNS-SPI download run)

try to start an ap with system no os .so add code to start ap ,but fail.

if ( wiced_wifi_start_ap( AP_SSID, AP_SEC, (uint8_t*) AP_PASS, sizeof( AP_PASS ) - 1, AP_CHANNEL ) != WICED_SUCCESS )

{

        WPRINT_APP_INFO(("Failed to start  : " AP_SSID "  .. retrying\r\n"));

}

the place of fail is at wiced_send_ioctl function

get log :

Received a response for a different IOCTL - retry

2 Replies
SeyhanA_31
Employee
Employee
100 likes received 50 likes received 25 likes received

Hi,

Did you resolve your issue by using OS and network stack?

Do you still have a question?

Seyhan

0 Likes

Dear Seyhan,

Don't have this issue by using os and network stack.

I have resolved this issue .

Thanks.

Best Regards

Chuang Chen

Shanghai R&D Center

Zhejiang Shenghui Lighting Co., Ltd

Tel: 021-60707500-8090

Mobile:18817395505

Email:chenc@sengled.com

发件人: seyhan

发送时间: 2015-01-08 10:07

收件人: chuang chen

主题: Re: - Can't start an AP with no OS and no network stack on platform of BCM943362WCD2 ?

Can't start an AP with no OS and no network stack on platform of BCM943362WCD2 ?

reply from seyhan in WICED Wi-Fi Forums - View the full discussion

Hi,

Did you resolve your issue by using OS and network stack?

Do you still have a question?

Seyhan

Reply to this message by replying to this email, or go to the message on Broadcom Community

Start a new discussion in WICED Wi-Fi Forums by email or at Broadcom Community

Following Can't start an AP with no OS and no network stack on platform of BCM943362WCD2 ? in these streams: Inbox

0 Likes