- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I'm not having any luck launching the debugger. It looked like I had it running for a while, although it never stopped on any of my breakpoints, so I'm not 100% confident.
I'm using a Murata SN8200EVK, and I've selected the following options on the debug configuration dialog:
Main:
C/C++ Application: build/myApps_myWebServer-SN8200x/Binary/myApps_myWebServer-SN8200x.elf
Project: Wiced-SDK
Build configuration: Use Active
Disable auto build
Debugger:
GDB Command: C:\Users\gluterman\Documents\WICED\WICED-SDK-2.4.1\Wiced-SDK\Tools\ARM_GNU\bin\Win32\arm-none-eabi-gdb.exe
Force thread list update on suspend
Startup:
Halt: add-symbol-file build/eclipse_debug/last_bootloader.elf 0x8000000
Load symbols: Use project binary
Run Commands: stepi
Source:
Default
Common:
Local file
When I try to run the debugger, I get: Error in final launch sequence
Details include Failed to execute MI command:stepiError message from debugger back end:The program is not being run
Any ideas what I'm doing wrong?
Also, we've had a lot of success using our IAR debugger for ARM in the past. Is it possible to use the IAR debugger with this device/library? Or is Eclipse the only way to go?
Thanks.
- Labels:
-
Debug
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Debugging Murata SN8200EVK works fine for me.
Please change C/C++ Application to "build/eclipse_debug/last_built.elf".
You may also take a look at Creating and/or Editing Debug Configurations as well.
Let me know if you still have issue for debugging.
Thanks,
Seyhan