Anonymous
Not applicable
Mar 18, 2013
07:42 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Mar 18, 2013
07:42 PM
[wiced-sdk-2.2.1, bcm43362]
Labels
- Tags:
- 11ga
- 802.11
- 802.bgn
- additional
- advertises
- bcm43362
- beacon
- bgn
- capabilities
- capability
- chip
- client
- coding
- configured
- displayed
- element
- elements
- exist
- extended
- field
- frames
- http:ccie-or-null.net20110622802-11-beacon-frames
- included
- includes
- info
- join
- mode
- modulation
- needed
- probes
- rates
- related
- scheme
- searching
- sets
- shown
- snippet
- softap
- supported
- transmit
- wiced
1 Reply
Anonymous
Not applicable
Mar 18, 2013
07:47 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Mar 18, 2013
07:47 PM
Yes. the BCM43362 is an 802.b/g/n chip.It is configured to use all b/g/n rates as and when needed (both in client and softAP mode).FYI, there are 12 b/g rates. Eight rates are displayed in the supported rates element which can be 11b or 11g/a. The additional 4 x g rates are displayed in the extendedsupported rates element if they exist. 11n rates are displayed as Modulation and Coding Scheme sets in the HT related elements.The softAP beacon advertises all b/g rates and includes the HT capabilities (11n) element.A snippet of info about beacon frames is shown herehttp://ccie-or-null.net/2011/06/22/802-11-beacon-framesFYI, the same HT capability field is included in 802.11 probes sent by the WICED client when searching for APs to join.