Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

I want to get the debug info in app wwd.canned_send from sdk 3.1.2.

I commented these lines in NoOS_canned_send.c:

/* In release builds all UART printing is TURNED OFF to remove printf and malloc dependency which reduces memory usage dramatically YIN REN ZHU MU DI */

//#ifndef DEBUG

//#undef  WPRINT_APP_INFO

//#define WPRINT_APP_INFO(args)

//#endif

other Code from the Wiced-SDK-3.1.2-IDE-Installer.exe are NOT modified.

I can NOT get the debug info yet from the WICED USB Serial Port( it can work well with other app) after making target.

open the declatration as follwing:

WPRINT_APP_INFO(("\nPlatform " PLATFORM " initialised\n"));

is

#define WPRINT_APP_INFO(args) WPRINT_MACRO(args)

is

#define WPRINT_MACRO(args) do {printf args;} while(0==1)


Could you please tell me what is wrong? I appreciate your help.

0 Likes
2 Replies
JaeyoungY_71
Employee
Employee
First comment on KBA 25 solutions authored 10 solutions authored

Hi,

You can undo(uncomment so code is not modified at all) the changes for the following and add "-debug" to your target name.

//#ifndef DEBUG

//#undef  WPRINT_APP_INFO

//#define WPRINT_APP_INFO(args)

//#endif

For instance, I used

"wwd.canned_send-BCM943362WCD4-NoOS-NoNS-debug download run"

as the target name on Wiced SDK 3.1.2 for BCM43362WCD4 board and I can see the info printed out. (I left the AP_SSID/AP_PASS as the default, you should change this to match your AP in the code though)

debug_info.PNG

Anonymous
Not applicable

Thanks a lot.

0 Likes