- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
right now im getting into the WLAN capabilities of the CYW54907 with said development board.
I use the Config_join_ping code example to get the basics, but a problem has occured for me.
My PC is in the network connected via ethernet.
The dev board is connected to the network via WLAN.
Both IPv4 and IPv6 are configured on PC and board.
Now when i ping the IPs, there are some problems coming up and right now im out of ideas what could cause them:
PC pings board with IPv4 -> answer
PC pings board with IPv6 -> answer
Board pings PC with IPv4 -> answer
Board pings PC with IPv6 -> packages lost
BUT: Colleagues PC pings my PC with IPv6 -> answer
So my PC can be pinged by another PC via IPv6, but when i try to ping the same IPv6 with the CYW954907AEVAL1F, i always loose 100% of the packages.
What could cause this behaviour? Is there anything else i neet set up to use IPv6 with the board?
EDIT: Seems i found one possible reason, the ping-command only resolves IPv4 ping attempts and it seems the IPv6 is converted wrong. Ill dig into that
Solved! Go to Solution.
- Labels:
-
Ethernet
-
TCPIP
-
Wi-Fi Direct
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
Ping for ipv6 is not implemented in WICED.
if ( address->version != WICED_IPV4 )
{
wiced_assert("ping for ipv6 not implemented yet", 0!=0);
return WICED_TCPIP_UNSUPPORTED;
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
Ping for ipv6 is not implemented in WICED.
if ( address->version != WICED_IPV4 )
{
wiced_assert("ping for ipv6 not implemented yet", 0!=0);
return WICED_TCPIP_UNSUPPORTED;
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello PriyaM,
ive seen that too, but forgot to edit the question. Thanks for answering and for the code snipped which specifies that.
Have a great day!