Good day, i have measured TCP transmission speed, and im very surprised.
I got only around 250KB/s, why speed is so slow, I tried 5G and 2.4G WIFI, transfered locally with 1Gb router?
Actually i tried to measure MicroSD speed and got good results.
I think 320-MHz Arm Cortex-R4 should be much faster...
Maybe Im doing something wrong?
Here is my code:
#include "wiced.h"
#define TCP_PACKET_MAX_DATA_LENGTH 1024
#define TCP_CLIENT_INTERVAL 10
#define TCP_SERVER_PORT 111
#define TCP_CLIENT_CONNECT_TIMEOUT 60000
#define TCP_CLIENT_RECEIVE_TIMEOUT 60000
#define TCP_CONNECTION_NUMBER_OF_RETRIES 10
#define TCP_SERVER_IP_ADDRESS MAKE_IPV4_ADDRESS(192,168,31,10)
static wiced_result_t tcp_client1();
static wiced_tcp_socket_t tcp_client_socket1;
#define TCP_SERVER_THREAD_PRIORITY (WICED_DEFAULT_LIBRARY_PRIORITY)
#define TCP_SERVER_STACK_SIZE (1024*10)
#define BUFFER_SIZE 512
typedef struct
{
wiced_bool_t quit;
wiced_tcp_socket_t socket;
}tcp_server_handle_t;
static wiced_thread_t tcp_thread1;
static tcp_server_handle_t tcp_server_handle1;
void application_start(void)
{
wiced_result_t result;
wiced_init( );
wiced_network_up( WICED_STA_INTERFACE, WICED_USE_EXTERNAL_DHCP_SERVER, NULL );
wiced_tcp_create_socket( &tcp_client_socket1, WICED_STA_INTERFACE);
wiced_tcp_bind( &tcp_client_socket1, TCP_SERVER_PORT );
wiced_rtos_create_thread(&tcp_thread1, TCP_SERVER_THREAD_PRIORITY, "speed_test", tcp_client1, TCP_SERVER_STACK_SIZE, &tcp_server_handle1);
WPRINT_APP_INFO(("\ntcp speed task created!"));
while(1);
}
wiced_result_t tcp_client1( void* arg )
{
wiced_result_t result;
wiced_packet_t* packet;
char* tx_data;
uint16_t available_data_length;
const wiced_ip_address_t INITIALISER_IPV4_ADDRESS( server_ip_address, TCP_SERVER_IP_ADDRESS );
int connection_retries;
char data_buffer[BUFFER_SIZE];
uint32_t i = 0;
wiced_time_t scan_start_time;
wiced_time_t scan_end_time;
UNUSED_PARAMETER( arg );
connection_retries = 0;
do
{
result = wiced_tcp_connect( &tcp_client_socket1, &server_ip_address, TCP_SERVER_PORT, TCP_CLIENT_CONNECT_TIMEOUT );
connection_retries++;
}
while( ( result != WICED_SUCCESS ) && ( connection_retries < TCP_CONNECTION_NUMBER_OF_RETRIES ) );
if( result != WICED_SUCCESS)
{
WPRINT_APP_INFO(("Unable to connect to the server! Halt.\n"));
}
if (wiced_packet_create_tcp(&tcp_client_socket1, TCP_PACKET_MAX_DATA_LENGTH, &packet, (uint8_t**)&tx_data, &available_data_length) != WICED_SUCCESS)
{
WPRINT_APP_INFO(("TCP packet creation failed\n"));
return WICED_ERROR;
}
for(i = 0; i < BUFFER_SIZE; i++)
{
data_buffer = 'w';
}
wiced_time_get_time(&scan_start_time);
i = 0;
while(1){
wiced_tcp_send_buffer( &tcp_client_socket1, &data_buffer[0], BUFFER_SIZE);
i++;
if(i >= 250){
i = 0;
wiced_time_get_time(&scan_end_time);
WPRINT_APP_INFO(("\nspeed: %d KBs", (int)(((BUFFER_SIZE*250000) / 1024) / (int)(scan_end_time - scan_start_time))));
wiced_time_get_time(&scan_start_time);
}
}
wiced_tcp_disconnect(&tcp_client_socket1);
return WICED_SUCCESS;
}
Solved! Go to Solution.
Based on my understanding, the TCP client application is a very basic application where you simply open a socket ,send the data, receive a response and disconnect; this will then repeat every 2 seconds. In contrast, It's my understanding that iperf will perform the data transfer in a single connection.
Essentially, the objective of the TCP client application is not really for performance measurement, but to demonstrate how to both use the WICED TCP client & how to communicate with a TCP server.
Again, we believe that the iperf client will send data over single connection, and the implementation will be more robust then our TCP client application.
I think it is better to describe your setup what you are communicating with and how, so that people can do the same test. How about trying iperf on test.console? A few MB/s is possible on 2.4GHz. What is your target throughput?
Hi,
Thank you for your answer.
With test.console and iperf I got 108 Mbit on 5Ghz and 45 Mb on 2.4Ghz.
Is there an example of FTP for example or other protocol to test?
With previous example I used my own server to test the speed.
Maybe with Iperf device uses different sending function than this:
wiced_tcp_send_buffer( &tcp_client_socket1, &data_buffer[0], BUFFER_SIZE);
Thanks.
Generally, we recommend to use iperf for TCP, UDP throughput. Indeed iperf uses different sending function than the wiced level TCP APIs.
Do you mean a normal application code using wiced API cannot reach the throughput as iperf does?
Then what is the expected best throughput using wiced API?
AFAICT, 45Mb v.s. 250KB is a huge gap.
I need to do more test to be more precise with my tests.
Because i write my own tcp server, not sure if its written right.
Will check it later.
Im thinking writing my own ftp client to check what speeds I will get.
Will post results later..
Is it possible somehow to use Iperf functions?
Thanks.
I am not sure about using Iperf functions. During our testing, we used the TCP Stream APIs (Detailed help article: TCP stream API ) to measure throughput between two 43907 platforms and the throughput was found to be 14.6 MBps
Based on my understanding, the TCP client application is a very basic application where you simply open a socket ,send the data, receive a response and disconnect; this will then repeat every 2 seconds. In contrast, It's my understanding that iperf will perform the data transfer in a single connection.
Essentially, the objective of the TCP client application is not really for performance measurement, but to demonstrate how to both use the WICED TCP client & how to communicate with a TCP server.
Again, we believe that the iperf client will send data over single connection, and the implementation will be more robust then our TCP client application.
Good day,
I did some testing with filezilla ftp server and got some not bad results. I got around 3.2MB/s
With bigger buffer buffer, In 1st example i used 1kb buffer, in second example i used 4kb data buffer, got better (4.3 MB data rate).