Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Wi-Fi Combo

mvpablo
Level 2
10 sign-ins 5 replies posted 5 questions asked
Level 2

Hi.

I'm trying to create a VERY SIMPLE app, where a user executes the following steps:

  1. From mobile or pc the user search for the board AP, finds the WICED and connects to it
  2. Open a browser types 192.168.0.1 and the browsers displays the wifi config page
  3. chooses a network, types credentials, submit
  4. the board connects to the network and saves the wifi profile.

So I tried to find documentation on how this whole Web Server, Wifi onboarding process work in WICED Studio WiFi and I couldn't find any detailed document with the explanation other than go to the examples.

I took the example snip/config_mode. ran it several times and all I get is this:

  1. The snip builds into the board
  2. from my laptop, I connect to the AP "WICED Config"
  3. Go to a browser and configure access to a wifi network.
  4. I get the IP (192.168.0.19) in the UART, that I double check it is also the one assigned by the wifi router
  5. I switch to the IP provided.
  6. web page doesn't load, stays forever and I don't get any feedback in the UART.

Questions: 

Is there anything that I'm missing here?

Is there any DETAILED documentation on how the wifi onboarding works?:  Something that tells me how to capture errors if I type the wrong credentials, manage different network profiles, stored them,  Where are the files to configure the web server, html files (I know they are in resouces/../...). I need guidance on how all those things are wired together.

Starting WICED Wiced_006.004.000.0061

Platform CYW943907AEVAL1F initialised

Started ThreadX v5.8

WICED_core Initialized

Initialising NetX_Duo v5.10_sp3

Creating Packet pools

WLAN MAC Address : C4:AC:59:98:AE:36

WLAN Firmware    : wl0: May  2 2019 02:34:15 version 7.15.168.130 (r714231) FWID 01-7fc7cd46

WLAN CLM         : API: 12.2 Data: 9.10.74 Compiler: 1.31.3 ClmImport: 1.36.3 Creation: 2019-05-02 02:29:29

IPv4 network ready IP: 192.168.0.1

Setting IPv6 link-local address

IPv6 network ready IP: FE80:0000:0000:0000:C4AC:59FF:FE98:AE36

Joining : intheairhome

Successfully joined : intheairhome

Obtaining IPv4 address via DHCP

L1420 : dhcp_client_init() : DHCP CLIENT hostname = [WICED IP]

IPv4 network ready IP: 192.168.0.19

Setting IPv6 link-local address

IPv6 network ready IP: FE80:0000:0000:0000:C6AC:59FF:FE98:AE36

Application DCT Configuration:

First Name = John

Last Name  = Citizen

Address 1  = Level 15

Address 2  = 24 Campbell St

Suburb     = Sydney

Country    = Australia

Zipcode    = 2000

Phone      = +612 5555 5555

thanks

0 Likes
1 Reply
YashM
Moderator
Moderator First question asked 250 sign-ins 100 replies posted
Moderator

Hi

1. After connecting to the WICED Config soft AP, you need to go to the browser and type wiced.com or 192.168.0.1 and the HTML page will load up (if the html doesn't load up then please try some other browser).

The HTML page with following details will load up.

pastedImage_0.png

Try changing one of the fields and save the settings. Click on Wi-Fi Setup and all the available APs will be scanned. Connect to your router (AP) by providing the password in the Wi-Fi setup itself, once connected you will be able to see the UART prints.

2. Regarding the documentation, we don't have any standard documentation, you have to understand the flow of code manually.

Thanks and Regards

Yash

0 Likes