Hi.
I have a program, which stream video over AP by (RTP+RTSP).
I have periodical task with frequency 40ms and it send about 9-10 packets with size 1300 per task execution.
All fine with unicast address eg. host have 192.168.10.1 and receiver 192.168.10.2.
But when I try to send UDP broadcast(192.168.10.255(mask 255.255.255.0) or WICED_IP_BROADCAST(255.255.255.255)) there is a lot of packets lost(up to 50%).
I try to uncomment NX_DISABLE_UDP_INFO , increase WICED_DEFAULT_UDP_QUEUE_SIZE from 5 to 20, reduce WICED_ALLOCATE_PACKET_TIMEOUT from 2000 to 30, but nothing help. There is no error occurs at send and no packet creation fails. Also I`ve tried to use different type_of_service for UDP socket. There is any difference in implementation of unicast/broadcast UDP packet send? Or someone have idea how to increase efficiency of UDP video streaming?
Thanks for answers!
Solved! Go to Solution.
I`ve made some tests.
Seems WiFi physical interface guarantees delivery of the package for unicast IP, even it is UDP packet on protocol layer.
I have 26 RTP-AP frame, which have about 15-17 separates packets. There is no packets lost, so video is fine, too.
But, when I try to send for broadcast, I have loss rate about 3-12% depended on distance, etc , and if only 1 packet in a frame is lost - all frame lost too for decoder on receiver side. That`s why video have lags. Even with good quality WiFi 3%*15=45% packets lost.
I`ve made some tests.
Seems WiFi physical interface guarantees delivery of the package for unicast IP, even it is UDP packet on protocol layer.
I have 26 RTP-AP frame, which have about 15-17 separates packets. There is no packets lost, so video is fine, too.
But, when I try to send for broadcast, I have loss rate about 3-12% depended on distance, etc , and if only 1 packet in a frame is lost - all frame lost too for decoder on receiver side. That`s why video have lags. Even with good quality WiFi 3%*15=45% packets lost.