- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I am able to write to a dev kit using a segger jlink, however when trying to program our custom hardware (which is very similar to the dev kit) it reads successfully the id 0x5BA00477 but quickly fails afterwards.
See output:
SEGGER J-Link Commander V7.63b (Compiled Mar 1 2022 16:42:47)
DLL version V7.63b, compiled Mar 1 2022 16:41:28
Connecting to J-Link via USB...O.K.
Firmware: J-Link V11 compiled Dec 9 2021 14:14:49
Hardware version: V11.00
S/N: 821008088
License(s): GDB
USB speed mode: High speed (480 MBit/s)
VTref=3.180V
Device "CYW43907" selected.
Connecting to target via JTAG
TotalIRLen = 4, IRPrint = 0x01
JTAG chain detection found 1 devices:
#0 Id: 0x5BA00477, IRLen: 04, CoreSight JTAG-DP
Identified core does not match configuration. (Found: None, Configured: Cortex-R4)
TotalIRLen = 4, IRPrint = 0x01
JTAG chain detection found 1 devices:
#0 Id: 0x5BA00477, IRLen: 04, CoreSight JTAG-DP
****** Error: Could not power up debug port: Control/Status register reads 00000F02
TotalIRLen = 4, IRPrint = 0x01
JTAG chain detection found 1 devices:
#0 Id: 0x5BA00477, IRLen: 04, CoreSight JTAG-DP
TotalIRLen = 4, IRPrint = 0x01
JTAG chain detection found 1 devices:
#0 Id: 0x5BA00477, IRLen: 04, CoreSight JTAG-DP
Cannot connect to target.
When looking at JTAG signals, we can see that the voltages are unexpected:
TDI/TMS: ~2.4V
TCK: ~2.5V
TDO/VTref: 3.3V
According to segger:
The J-Link has 100 Ohm serial resistors at TDI/TMS and 68 Ohm at TCK.
The voltage drop at TDI/TMS is 0.9V with 9mA load current
The voltage drop at TCK is 0.7V with 9mA load current
According to CYW43907 doc:
GPIO have programmable 2 mA to 16 mA drive strength. Default is 10 mA
Are the GPIOs set as output to GND with an empty flash?
Solved! Go to Solution.
- Labels:
-
ispn:36623:1:0
-
l1:3966:1:0
-
l2:6066:1:0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
You can close this, it was a wiring mistake on the jlink (nTRST connected to ground)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
You can close this, it was a wiring mistake on the jlink (nTRST connected to ground)