- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
What should I be seeing for throughput from iperf and a CYW43907?
Iperf client is on CYW43907 and the server is on PC. The test is over UDP.
CYW43907 is wireless (5GHz) through router to computer (Ubuntu) over Ethernet.
The CYW43907 is within 5 feet of the router and the channel appears relatively unused.
The server is running iperf version 2.0.4+svnr43
The iperf code in WICED appears to be based on 2.0.5
Commands:
iperf -u -c 192.168.1.110 (client)
iperf -u -s (server)
Test app is based on SDK 6.2
Results
FreeRTOS + LwIP
------------------------------------------------------------
Client connecting to 192.168.1.110, UDP port 5001
Sending 1470 byte datagrams
UDP buffer size: 8.55 KByte (default)
------------------------------------------------------------
[ ID] Interval Transfer Bandwidth
[ 0] 0.0-10.0 sec 1.25 MBytes 1.05 Mbits/sec
[ 0] Sent 893 datagrams
[ 0] Server Report:
[ 0] 0.0-10.0 sec 1.25 MBytes 1.05 Mbits/sec 0.503 ms 1/ 894 (0.11%)
Thread X + NetX
------------------------------------------------------------
Client connecting to 192.168.1.110, UDP port 5001
Sending 1470 byte datagrams
UDP buffer size: 7.81 KByte (default)
------------------------------------------------------------
[ ID] Interval Transfer Bandwidth
[ 0] 0.0-10.0 sec 1.25 MBytes 1.05 Mbits/sec
[ 0] Sent 893 datagrams
[ 0] Server Report:
[ 0] 0.0-10.0 sec 1.25 MBytes 1.05 Mbits/sec 0.482 ms 1/ 894 (0.11%)
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Here is the table for throughput values of CYW43907.
WICED version: 6.2
Access Point: NETGEAR, 5GHz band
iperf version : 2.0.9
Make Target: test.console-CYW943907AEVAL1F download run
Note: These values are observed when measured in RF box with no interference.