Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
SeSo_4694526
Level 2
Level 2

Hello, we've had some breakthroughs with the configuration of our module CYW43455 on our custom board. We've been able to setup an Access Point on the 5Ghz band and it was possible to connect to it and have traffic to the internet via the wan interface.

But now we need also to setup the 2.4 Ghz band, and the situation here es that we don't see it available on the Openwrt Wireless Overview

Now, our question would be if it is necessary to do something in particular to startup the second radio for the other band, or if it should start automatically, then what could we be missing this time?

Thank you.

0 Likes
1 Solution
kama_1693131
Level 5
Level 5
Distributor - Marubun (Japan)
50 sign-ins 25 sign-ins 10 likes received

Hi SeSo,

Thank you for your sharing information.

I think your system failed download the nvram.

Your driver(brcmfmac) try to download following nvram to CYW43455.

It does not download brcmfmac43455-sdio.txt.

>brcmfmac43455-sdio.atmel,sama5d27-som1-ek.txt

How about rename brcmfmac43455-sdio.1MW.txt to brcmfmac43455-sdio.atmel,sama5d27-som1-ek.txt?

It is seems your brcmfmac source has modified for your custom board to find above nvram name.

Regards,

Matayoshi

View solution in original post

13 Replies
SeSo_4694526
Level 2
Level 2

Luci

pastedImage_0.png

0 Likes
kama_1693131
Level 5
Level 5
Distributor - Marubun (Japan)
50 sign-ins 25 sign-ins 10 likes received

Hi SeSo,

Do you want to use CYW43455 both 2.4GHz AP and 5GHz AP concurrently?

CYW43455 does not supported dual band AP concurrently.

Cypress called this feature RSDB:Realtime simultaneous dual band.

CYW43455 does not supported RSDB.

Regards,

Matayoshi

Ok thanks for your response

I try to change AP from 5GHz to 2.4GHz in /etc/config/wireless

config wifi-device 'radio0'

        option type 'mac80211'

        option path 'platform/ahb/b0000000.sdio-host/mmc_host/mmc1/mmc1:0001/mmc1:0001:1'

        option hwmode '11b'

        option htmode 'HT20'

        option channel '6'

config wifi-iface 'default_radio0'

        option device 'radio0'

        option mode 'ap'

        option network 'DR450'

        option ssid 'DR450'

        option key 'DetecDR450'

        option encryption 'psk2'

this is the response, appears in radio0 "device is not active"pastedImage_0.png

0 Likes

If I change the /etc/config/wireless to the following setup works in 5GHz

config wifi-device 'radio0'
        option type 'mac80211'
        option path 'platform/ahb/b0000000.sdio-host/mmc_host/mmc1/mmc1:0001/mmc1:0001:1'
        option htmode 'VHT80'
        option channel '36'
        option hwmode '11a'

config wifi-iface 'default_radio0'
        option device 'radio0'
        option mode 'ap'
        option network 'DR450'
        option ssid 'DR450'
        option key 'DetecDR450'
        option encryption 'psk2'
        option wds '1'

0 Likes
kama_1693131
Level 5
Level 5
Distributor - Marubun (Japan)
50 sign-ins 25 sign-ins 10 likes received

Hi SeSo,

I understood what is your problem.

Your CYW43455 does not work 2.4GHz AP, but it works 5GHz.

Could you try to use it with following option?

I modified hwmode,channel and country.

config wifi-device 'radio0'

        option type 'mac80211'

        option hwmode '11g'

        option path 'platform/ahb/b0000000.sdio-host/mmc_host/mmc1/mmc1:0001/mmc1:0001:1'

        option htmode 'HT20'

        option channel 'auto'

        option country 'US'

If it does not affect on your environment,

could you share your FW,nvram,clm_blob and driver information?

Regards,

Matayoshi

0 Likes

This is the output of dmesg with the firmware version and name

[    8.330000] brcmfmac: brcmf_fw_alloc_request: using brcm/brcmfmac43455-sdio for chip BCM4345/6

[    8.390000] brcmfmac mmc1:0001:1: Direct firmware load for brcm/brcmfmac43455-sdio.atmel,sama5d27-som1-ek.txt failed with error -2

[    8.400000] brcmfmac mmc1:0001:1: Falling back to user helper

[    8.450000] firmware brcm!brcmfmac43455-sdio.atmel,sama5d27-som1-ek.txt: firmware_loading_store: map pages failed

[    8.630000] brcmfmac: brcmf_fw_alloc_request: using brcm/brcmfmac43455-sdio for chip BCM4345/6

[    8.670000] brcmfmac: brcmf_c_preinit_dcmds: Firmware: BCM4345/6 wl0: Mar  1 2015 07:29:38 version 7.45.18 (r538002) FWID 01-6a2c8ad4

we downloaded brcmfmac43455-sdio.1MW.txt from GitHub and saved it on /lib/firmware/brcm, this allowed us to start using the 5Ghz band:

https://github.com/murata-wireless/cyw-fmac-nvram

Then the file was renamed to:

brcmfmac43455-sdio.txt

This is the content of the file:

# Cloned from bcm94345wlpagb.txt

NVRAMRev=$Rev: 498373 $

sromrev=11

vendid=0x14e4

devid=0x43ab

manfid=0x2d0

prodid=0x06e4

macaddr=00:90:4c:c5:12:38

nocrc=1

boardtype=0x6e4

##boardrev - superseded by the one in OTP

boardrev=0x1100

xtalfreq=37400

## tune where necessary

#xtal_swcapio=0x6644

boardflags=0x00080201

boardflags2=0x40000000

boardflags3=0x48200100

rxchain=1

txchain=1

aa2g=1

aa5g=1

tssipos5g=1

tssipos2g=1

AvVmid_c0=0,157,1,126,1,126,1,126,1,126

pa2ga0=-152,5969,-666

pa2ga1=-143,4076,-546

pa5ga0=-165,5736,-689,-169,5710,-692,-171,5713,-688,-173,5732,-689

#pa5ga1=-161,3672,-510,-166,3671,-508,-169,3697,-508,-171,3854,-520

itrsw=1

pdoffset40ma0=0x9999

pdoffset80ma0=0x8888

extpagain5g=2

extpagain2g=2

maxp2ga0=74

cckbw202gpo=0x0000

ofdmlrbw202gpo=0x0022

dot11agofdmhrbw202gpo=0x8888

mcsbw202gpo=0xaaaaa666

maxp5ga0=76,76,76,76

mcsbw205glpo=0x99999955

mcsbw205gmpo=0x99999955

mcsbw205ghpo=0x99999955

mcsbw405glpo=0xff999555

mcsbw405gmpo=0xff999555

mcsbw405ghpo=0xff999555

mcsbw805glpo=0xfffffbbb

mcsbw805gmpo=0xfffffbbb

mcsbw805ghpo=0xfffffbbb

swctrlmap_2g=0x00040004,0x00020002,0x00040004,0x010a02,0x1ff

swctrlmap_5g=0x00100010,0x00200020,0x00200020,0x010a02,0x2f4

swctrlmapext_5g=0x00000000,0x00000000,0x00000000,0x000000,0x000

swctrlmapext_2g=0x00000000,0x00000000,0x00000000,0x000000,0x000

vcodivmode=1

##filter parameters -- tune where necessary

cckdigfilttype=6

fdss_level_2g=2

fdss_level_5g=2

## added by apps

aga0=0x1

agbg0=0x1

ccode=0

ed_thresh2g=-65

ed_thresh5g=-65

ltecxmux=0

ltecxpadnum=0x0504

ltecxfnsel=0x22

ltecxgcigpio=0x32

pdoffsetcckma0=0x0000

powoffs2gtna0=0,0,0,0,0,0,0,0,0,0,0,0,0,0

tempthresh=120

temps_hysteresis=15

rawtempsense=0x1ff

tworangetssi2g=1

tworangetssi5g=0

lowpowerrange2g=0

lowpowerrange5g=0

ag0=1

ag1=1

#subband5gver=0x4

mcslr5glpo=0x0000

mcslr5gmpo=0x0000

mcslr5ghpo=0x0000

sb20in40hrpo=0x0

sb20in80and160hr5glpo=0x0

sb40and80hr5glpo=0x0

sb20in80and160hr5gmpo=0x0

sb40and80hr5gmpo=0x0

sb20in80and160hr5ghpo=0x0

sb40and80hr5ghpo=0x0

sb20in40lrpo=0x0

sb20in80and160lr5glpo=0x0

sb40and80lr5glpo=0x0

sb20in80and160lr5gmpo=0x0

sb40and80lr5gmpo=0x0

sb20in80and160lr5ghpo=0x0

sb40and80lr5ghpo=0x0

dot11agduphrpo=0x0

dot11agduplrpo=0x0

phycal_tempdelta=25

temps_period=15

btc_mode=1

sbpowoffs5g20mtna0=0,0,0,0

sbpowoffs5g40mtna0=0,0,0,0

sbpowoffs5g80mtna0=0,0,0,0

powoffs5g20mtna0=0,0,0,0,0,0,0

powoffs5g40mtna0=0,0,0,0,0

powoffs5g80mtna0=0,0,0,0,0

ldo1=5

cbfilttype=2

xtal_swcapio=0x8855

fdss_level_ch13=1,1

# muxenab defined to enable OOB IRQ. Level sensitive interrupt via WL_HOST_WAKE line.

muxenab=0x10

After we copied the file brcmfmac43455-sdio.clm_blob fromhttps://github.com/LibreELEC/brcmfmac_sdio-firmware-rpi/tree/master/firmware/brcm

brcmfmac_sdio-firmware-rpi/firmware/brcm at master · LibreELEC/brcmfmac_sdio-firmware-rpi · GitHub

That's about all the information we have.

Thank you

0 Likes
kama_1693131
Level 5
Level 5
Distributor - Marubun (Japan)
50 sign-ins 25 sign-ins 10 likes received

Hi SeSo,

Thank you for your sharing information.

I think your system failed download the nvram.

Your driver(brcmfmac) try to download following nvram to CYW43455.

It does not download brcmfmac43455-sdio.txt.

>brcmfmac43455-sdio.atmel,sama5d27-som1-ek.txt

How about rename brcmfmac43455-sdio.1MW.txt to brcmfmac43455-sdio.atmel,sama5d27-som1-ek.txt?

It is seems your brcmfmac source has modified for your custom board to find above nvram name.

Regards,

Matayoshi

We rename the brcmfmac43455-sdio.1MW.txt to brcmfmac43455-sdio.atmel,sama5d27-som1-ek.txt

This is the output of dmesg (the error gone)

[    8.360000] brcmfmac: brcmf_fw_alloc_request: using brcm/brcmfmac43455-sdio for chip BCM4345/6

[    8.600000] brcmfmac: brcmf_fw_alloc_request: using brcm/brcmfmac43455-sdio for chip BCM4345/6

[    8.630000] brcmfmac: brcmf_c_preinit_dcmds: Firmware: BCM4345/6 wl0: Mar  1 2015 07:29:38 version 7.45.18 (r538002) FWID 01-6a2c8ad4

But we have same problem CYW43455 does not work 2.4GHz AP, but it works 5GHz.

Thanks for your help

0 Likes

I don't know if we are using the correct configuration in NVRAM file

0 Likes
kama_1693131
Level 5
Level 5
Distributor - Marubun (Japan)
50 sign-ins 25 sign-ins 10 likes received

Hi SeSo,

Thank you for your confirmation.

>I don't know if we are using the correct configuration in NVRAM file

If you are using muRata 1MW module, you should use following nvram.

It does not disabled 2.4GHz.

brcmfmac43455-sdio.1MW.txt

Could you confirm your board's regulatory setting?

Please share your return value with following commands?

$iw reg get

$iw phy

Regards,

Matayoshi

0 Likes

Thanks

I confirm that we are using brcmfmac43455-sdio.1MW.txt

root@OpenWrt:~# iw reg get

global

country 00: DFS-UNSET

        (2402 - 2472 @ 40), (N/A, 20), (N/A)

        (2457 - 2482 @ 20), (N/A, 20), (N/A), AUTO-BW, PASSIVE-SCAN

        (2474 - 2494 @ 20), (N/A, 20), (N/A), NO-OFDM, PASSIVE-SCAN

        (5170 - 5250 @ 80), (N/A, 20), (N/A), AUTO-BW

        (5250 - 5330 @ 80), (N/A, 20), (0 ms), DFS, AUTO-BW, PASSIVE-SCAN

        (5490 - 5730 @ 160), (N/A, 20), (0 ms), DFS, PASSIVE-SCAN

        (5735 - 5835 @ 80), (N/A, 20), (N/A), PASSIVE-SCAN

        (57240 - 63720 @ 2160), (N/A, 0), (N/A)

root@OpenWrt:~# iw phy

Wiphy phy0

        max # scan SSIDs: 10

        max scan IEs length: 2048 bytes

        max # sched scan SSIDs: 16

        max # match sets: 16

        max # scan plans: 1

        max scan plan interval: 508

        max scan plan iterations: 0

        Retry short limit: 7

        Retry long limit: 4

        Coverage class: 0 (up to 0m)

        Device supports roaming.

        Device supports T-DLS.

        Available Antennas: TX 0 RX 0

        Supported interface modes:

                 * IBSS

                 * managed

                 * AP

                 * P2P-client

                 * P2P-GO

                 * P2P-device

        Band 1:

                Capabilities: 0x1022

                        HT20/HT40

                        Static SM Power Save

                        RX HT20 SGI

                        No RX STBC

                        Max AMSDU length: 3839 bytes

                        DSSS/CCK HT40

                Maximum RX AMPDU length 65535 bytes (exponent: 0x003)

                Minimum RX AMPDU time spacing: 16 usec (0x07)

                HT TX/RX MCS rate indexes supported: 0-7

                Frequencies:

                        * 2412 MHz [1] (20.0 dBm)

                        * 2417 MHz [2] (20.0 dBm)

                        * 2422 MHz [3] (20.0 dBm)

                        * 2427 MHz [4] (20.0 dBm)

                        * 2432 MHz [5] (20.0 dBm)

                        * 2437 MHz [6] (20.0 dBm)

                        * 2442 MHz [7] (20.0 dBm)

                        * 2447 MHz [8] (20.0 dBm)

                        * 2452 MHz [9] (20.0 dBm)

                        * 2457 MHz [10] (20.0 dBm)

                        * 2462 MHz [11] (20.0 dBm)

                        * 2467 MHz [12] (disabled)

                        * 2472 MHz [13] (disabled)

                        * 2484 MHz [14] (disabled)

        Band 2:

                Capabilities: 0x1062

                        HT20/HT40

                        Static SM Power Save

                        RX HT20 SGI

                        RX HT40 SGI

                        No RX STBC

                        Max AMSDU length: 3839 bytes

                        DSSS/CCK HT40

                Maximum RX AMPDU length 65535 bytes (exponent: 0x003)

                Minimum RX AMPDU time spacing: 16 usec (0x07)

                HT TX/RX MCS rate indexes supported: 0-7

                VHT Capabilities (0x00001020):

                        Max MPDU length: 3895

                        Supported Channel Width: neither 160 nor 80+80

                        short GI (80 MHz)

                        SU Beamformee

                VHT RX MCS set:

                        1 streams: MCS 0-9

                        2 streams: not supported

                        3 streams: not supported

                        4 streams: not supported

                        5 streams: not supported

                        6 streams: not supported

                        7 streams: not supported

                        8 streams: not supported

                VHT RX highest supported: 0 Mbps

                VHT TX MCS set:

                        1 streams: MCS 0-9

                        2 streams: not supported

                        3 streams: not supported

                        4 streams: not supported

                        5 streams: not supported

                        6 streams: not supported

                        7 streams: not supported

                        8 streams: not supported

                VHT TX highest supported: 0 Mbps

                Frequencies:

                        * 5170 MHz [34] (disabled)

                        * 5180 MHz [36] (20.0 dBm)

                        * 5190 MHz [38] (disabled)

                        * 5200 MHz [40] (20.0 dBm)

                        * 5210 MHz [42] (disabled)

                        * 5220 MHz [44] (20.0 dBm)

                        * 5230 MHz [46] (disabled)

                        * 5240 MHz [48] (20.0 dBm)

                        * 5260 MHz [52] (20.0 dBm) (no IR, radar detection)

                        * 5280 MHz [56] (20.0 dBm) (no IR, radar detection)

                        * 5300 MHz [60] (20.0 dBm) (no IR, radar detection)

                        * 5320 MHz [64] (20.0 dBm) (no IR, radar detection)

                        * 5500 MHz [100] (20.0 dBm) (no IR, radar detection)

                        * 5520 MHz [104] (20.0 dBm) (no IR, radar detection)

                        * 5540 MHz [108] (20.0 dBm) (no IR, radar detection)

                        * 5560 MHz [112] (20.0 dBm) (no IR, radar detection)

                        * 5580 MHz [116] (20.0 dBm) (no IR, radar detection)

                        * 5600 MHz [120] (20.0 dBm) (no IR, radar detection)

                        * 5620 MHz [124] (20.0 dBm) (no IR, radar detection)

                        * 5640 MHz [128] (20.0 dBm) (no IR, radar detection)

                        * 5660 MHz [132] (20.0 dBm) (no IR, radar detection)

                        * 5680 MHz [136] (20.0 dBm) (no IR, radar detection)

                        * 5700 MHz [140] (20.0 dBm) (no IR, radar detection)

                        * 5720 MHz [144] (20.0 dBm) (no IR, radar detection)

                        * 5745 MHz [149] (20.0 dBm)

                        * 5765 MHz [153] (20.0 dBm)

                        * 5785 MHz [157] (20.0 dBm)

                        * 5805 MHz [161] (20.0 dBm)

                        * 5825 MHz [165] (20.0 dBm)

        valid interface combinations:

                 * #{ managed } <= 1, #{ P2P-device } <= 1, #{ P2P-client, P2P-GO } <= 1,

                   total <= 3, #channels <= 2

                 * #{ managed } <= 1, #{ AP } <= 1, #{ P2P-client } <= 1, #{ P2P-device } <= 1,

                   total <= 4, #channels <= 1

        Supported extended features:

                * [ DFS_OFFLOAD ]: DFS offload

root@OpenWrt:~#

0 Likes
kama_1693131
Level 5
Level 5
Distributor - Marubun (Japan)
50 sign-ins 25 sign-ins 10 likes received

Hi SeSo,

Thank you for checking it.

Your regulatory setting is not limited operation band.

In some cases, the setting of clm_blob may limit the operation.

Could you try to use latest clm_blob from below?

Cypress Linux WiFi Driver Release (FMAC) [2020-04-02]

/cypress-fmac-v5.4.18-2020_0402/firmware/brcmfmac43430-sdio.clm_blob

Regards,

Matayoshi

0 Likes

You will want to reach out to Murata (ToIn_1742091​) for the latest CLM BLOB/NVRAM that's been optimized for their Type 1MW module and the associated regulatory for the regions the module supports.

0 Likes