- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Is there a bug in the `gpio_button_init` function?
The code is:
return wiced_gpio_init( button->gpio, ( button->polarity == WICED_ACTIVE_HIGH )? INPUT_PULL_UP: INPUT_PULL_DOWN );
If a button is set up as active-low, so that the GPIO is connected to ground went it is pressed, shouldn't the micro therefor provide a pull UP, to restore the input to the non-active state?
And vice versa for active-high: GPIO goes high while button is pressed, then a pull DOWN is needed to return it to inactive when the button is released.
I ran into this when trying to set up the button_manager in SDK 5.1 .
Solved! Go to Solution.
- Labels:
-
GPIO
- Tags:
- button
- push button
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
Hi Andrew:
I will look into this case, by the way do you meet some issues when you configure the GPIO functions?
and which evb or chip you are using now?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
The issue that I was seeing was that that the on-chip PU/PD was not being activated correctly.
Patching this line to:
return wiced_gpio_init( button->gpio, ( button->polarity == WICED_ACTIVE_HIGH )? INPUT_PULL_DOWN: INPUT_PULL_UP );
and corresponding changes in gpio_button_enable() and wiced_gpio_input_get() make my configuration with button_manager work as expected. On chip PU is switched on, IRQ's are called, and click/hold/double click events are detectable.
I hope I am not missing something obvious; this logic just appears to be inverted, but consistently through the gpio_button library.
I'm not using an EVM, I am working on custom-designed hardware (product prototype). The micro is STM32F4.
A separate but follow-up issue I have is that button manager does perform too well in the presence of certain noise or slow rising edges for an active-low button, and detects 0 or 1ms duration events rather than a qualifying "click" event. I will follow up with scope traces, if I get a chance.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Yes that is a bug
I filed an internal case.
Alan