Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
ChMa_3922746
Level 5
Level 5
10 likes received 10 likes given 5 likes given

On a factory fresh board with a Murata 1GC installed on it (CYW43907 chip) and a blank SPI EEPROM, is anything other than the WICED SDK and a JTAG interface needed to put all the software/firmware (incl. Murata WIFI fw) on the board and have it boot?

Put another way, if a factory fresh board is connected only via JTAG to the WICED SDK (via the appropriate dongle, such as on the EVAL board), is that enough to boot it and have it run regular software?

Thanks!

0 Likes
1 Solution
Zhengbao_Zhang
Moderator
Moderator
Moderator
250 sign-ins First comment on KBA 10 questions asked

Hello:

    If you want to flash the board, I think JTAG interface is needed. via the appropriate dongle , this is correct.

For Wiced SDK we don't need it always because we can download the flash by script also..

View solution in original post

2 Replies
Zhengbao_Zhang
Moderator
Moderator
Moderator
250 sign-ins First comment on KBA 10 questions asked

Hello:

    If you want to flash the board, I think JTAG interface is needed. via the appropriate dongle , this is correct.

For Wiced SDK we don't need it always because we can download the flash by script also..

Perfect, thank you.

0 Likes