Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Wi-Fi Combo Forum Discussions

Anonymous
Not applicable

I am using the Avnet AES-BCM4343W eval board and our project requires that the serial debug port be bi-directional.

Does the "WICED USB Serial Port" support bi-direction or is it output only from an eval board.

If it does support 2-way communication where/what is the api for the board to receive data from the serial port?

If it does not support 2-way communication can the code be modified to do so?

-Matt

0 Likes
1 Solution
Anonymous
Not applicable

Yes this is a fully bidirectional port


Lol at the sample console or uart applications in the sdk

View solution in original post

2 Replies
Anonymous
Not applicable

Yes this is a fully bidirectional port


Lol at the sample console or uart applications in the sdk

You can find the libraries for it in library->utilities->command_console