Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
GrahamS_21
Employee
Employee
25 replies posted 10 likes received 10 replies posted

I'm trying to run the snip.bluetooth.bt_dualmode_server project.

I have tried downloading on the the BCM94343W_AVN board and the Future Electronics NEB1DX_01 board (modifying the mk file for the avn project) shown here: NEB1DX-01 | Nebula 1.0 IoT Cloud Ready Development Board for IoT Applications | FUTURE ELECTRONICS D...

The project builds and downloads ok, but if i try to connect using the SPP Pro app on Android (using a stock Nexus 6 running Android 7.1.1) i can pair to the device but not connect to it.

I have attached the terminal logs from both projects in case they could be of any use. Is there something i need to do to get the project working?

This was tested on WICED 6.0.1.5

Thanks

Graham

1 Reply
algic_2862441
Level 1
Level 1
First like given

I have the same issue with the BCM94343WWCD1_EVB.

Thanks,

Alberto

0 Likes