I just got the latest SDK 3.7.0-3 and with this version the BLE stack does not work anymore.
After initialising the stack, I try to scan devices but instead of receiving scan results I get several time the event code BTM_ENABLED_EVT with the status code 0x2 (TIMEOUT) and then 0x1 (PENDING).
Platform: BCM943907AEVAL2F_1
BCM943907 is a WIFI only part. I'm not sure how you are managing to use it for BLE. Is the platform that you mentioned the correct one ?
When opening the schematics (platforms/BCM943907AEVAL2F_1/schematics/bcm943907aeval2f_p102.pdf) it is clearly written that the chip is a "BCM43907 & BCM20707- based SiP" and this board works like a charm with version 3.7.0.
So this is a regression report (works in sdk-3.7.0, but does not work in sdk-3.7.0-3)?
Yes it is, it used to work in 3.7.0 and I now have issues with 3.7.0-3
Hello, I come back to this issue as it still occurs in SDK 4.0.0.
When initializing the stack, I will first receive a BTM_ENABLED_EVT 0x0 (SUCCESS).
But then, if I start a scan: around 50% of the time, I won't receive any scan results and the management callback is called with BTM_ENABLED_EVT 0x2 (TIMEOUT).
I really cannot guess what's the behaviour of the stack as the source code is not provided at all.
marmottus wrote:
Hello, I come back to this issue as it still occurs in SDK 4.0.0.
When initializing the stack, I will first receive a BTM_ENABLED_EVT 0x0 (SUCCESS).
But then, if I start a scan: around 50% of the time, I won't receive any scan results and the management callback is called with BTM_ENABLED_EVT 0x2 (TIMEOUT).
I really cannot guess what's the behaviour of the stack as the source code is not provided at all.
The issue persists with SDK 4.0.1