Hi,
I am using BCM9WCD1EVAL1(P100) evaluation board with BCM943362WCD4(P200) ,But there is no schematic available for BCM9WCD1EVAL1(P100) in
"\WICED-SDK-3.5.2\WICED-SDK\platforms\evaluation_boards\BCM9WCD1EVAL1\schematics",
Where should i look for schematic of BCM9WCD1EVAL1(P100)
Or is there any other schematic similar to this ..
I found the schematic for BCM943362WCD4(P200).
Thanks,
Krishna.
Solved! Go to Solution.
I believe this is what you need: BCM43362 Evaluation Board Schematic (PDF)
Hi mwf_mmfae
In .../platforms/evaluation_boards/BCM9WCD1EVAL1/schematics directory there is no schematic for my "BCM9WCD1EVAL1(P100)" evaluation board .
All i found there is schematics for BCM9WCD1EVAL1_P200,BCM9WCD1EVAL1_P300,BCM9WCD1EVAL1_P400,P401,P402etc..
I need evaluation board schematic for
"BCM9WCD1EVAL1_P100"
Hi,
Base board schematics are part of the SDK, .../platforms/evaluation_boards.
Depending on the version of the BCM43362 base board, the schematics are located as part of the SDK in .../platforms/evaluation_boards/BCM9WCD1EVAL1/schematics directory.
Seyhan
Hi seyhan
I searched in .../platforms/evaluation_boards/BCM9WCD1EVAL1/schematics directory. but i didn't find schematic threre...
But you shared previously link is the one i needed.
Thanks.
I need to know that which pins are mapped where in the Expansion Header J7..
I am using BCM9WCD1EVAL1 _P100 with BCM943362WCD4 module on it...
I believe this is what you need: BCM43362 Evaluation Board Schematic (PDF)
I have "BCM43362 Evaluation Board Schematic (PDF)" this already
But i need the pin mapping of expansion header J7 Of "BCM9WCD1EVAL1 _P100" with "BCM943362WCD4 module" on it..
All i need is "Breakout Header pin mapping" of the BCM9WCD1EVAL1 _P100 evaluation board....
Is this what you are looking for?
Yes ,But this is for other eval board ...i will send snap of my eval board...
Here are the snaps of EVAL Board
which schematic should i refer ..
<<<<which schematic should i refer ..
On 8/22 I provided the Revision P100 schematics. Are you finding them inaccurate?
Hi,
Schematic attached with "BCM9WCD1EVAL1_P100.pdf" name is for the baseboard (black colored board.)
The red colored board schematic is released as part of the SDK, .../platforms/BCM943362WCD4/schematics/BCM943362WCD4_P200.pdf.
Seyhan