BCM943362WCD Atmel "bricked" issue

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

I was using Wiced 2.3.1 on a WCD8 eval board, running ping_powersave.  This all worked OK.  

I changed the WCD8 makefile to enable wait_mode_support, according to the Readme.txt.

* ^BCM943362WCD8 : OpenOCD Limitations with Power Save

      OpenOCD is unable to wake up and halt the ARM Cortex-M3 CPU of the AT91SAM4S

      MCU when the MCU enters deep sleep mode. Consequently, the powersave feature

      for BCM943362WCD8 is disabled by default. It can be enabled by uncommenting

      GLOBAL_DEFINES += WAIT_MODE_SUPPORT in <WICED-SDK>/Wiced/Platform/BCM943362WCD8/BCM943362WCD8.mk.

      This issue will be addressed in a future SDK release.

After this, I got OpenOCD errors.

**** OpenOCD failed - ensure you have installed the driver from the drivers directory, and that the debugger is not running **** In Linux this may be due to USB access permissions. In a virtual machine it may be due to USB passthrough settings. Check in the task list that another OpenOCD process is not running. Check that you have the correct target and JTAG device plugged in. ****"

I tried a clean build, unplugged/plugged the board, rebooted PC, no luck.

I tried a USI09 eval board, it worked fine.

Any idea why the Atmel SAM4 board appears to be bricked?

0 Likes
1 Reply
Anonymous
Not applicable
The problem is almost certainly that the SAM4S is in low power WAIT_MODE and will not respond to the JTAG interface.

The solution is to pull the flash ERASE pin of the MCU high for >220ms as noted on Page 28 of the SAM4 datasheet.
0 Likes