Hi everyone,
I need high power sdio 2.4g 1T1R wifi module in my project. But can not find it.
Now I want to use bcm43362 wifi chip with external PA to extand signal distance. The rf output is 23 - 25dbm.
The internal PA output in bcm43362 is 14dbm and can't satisfied this target. The rf input of external PA is as low to -3dbm so bypass the internal PA is the only way.
Does anybody know how to bypass the internal PA of bcm43362?
Solved! Go to Solution.
Did you try using wwd_wifi_set_tx_power() to adjust the tx power level?
We do not recommend changing the power settings because the product is shipped to countries keeping in mind regulatory compliance of each country. Please refer to the following threads:
This answer can not satisfy me, I need method of by pass the internal PA. Can I get the real answer.
Did you try using wwd_wifi_set_tx_power() to adjust the tx power level?
not sure if it's gonna function as well