Hello Support,
I am evaluating the platform CYW94343WWCD1 for power save and WLAN+BLE coex with power save.
I am using the WICED SDK version 6.0.1.5 and the latest 6.2.
while I am trying to download the code of test.powersave(used for taking standby associated power numbers) and demo.ble_wifi_introducer(used for the WLAN+BLE coex app), I am not able to do so.
I am getting an error saying that:
"
tools/makefiles/wiced_config.mk:428: *** powersave application does not support BCM94343WWCD1 platform. Stop.
make: *** No rule to make target 'build/test.powersave-BCM94343WWCD1-ThreadX-NetX/config.mk', needed by 'main_app'. Stop.
19:37:02 Build Finished (took 219ms)
"
I am attaching the snap-shot from both SDKs FYR.
Can you please help me with this? Why can not these applications be supported for this platform? Do I need to do some more setting to make these applications compatible?
Thanks
Akash
Solved! Go to Solution.
cool.milu69_3789331 wrote:
Hello,
Thanks for the reply.
I tried changing the makefile as below.
I am getting some other compilation errors. I even tried including header
file but no luck.
Added the platform BCM94343WWCD1 in the valid platform list.
Makefile:
Define as 1 if want to include WL commands into application
CONSOLE_ENABLE_WL := 0
VALID_PLATFORMS := BCM943909* BCM943907* BCM943903* CYW943907*
BCM4343W* BCM94343WWCD1*
INVALID_PLATFORMS := BCM943909QT
Compilation Error:
Making test.powersave-BCM94343WWCD1.elf
build/test.powersave-BCM94343WWCD1/libraries/App_powersave.a(powersave.o):
In function `startup_commands':
C:\Users\milan\Documents\WICED-Studio-6.0\43xxx_Wi-Fi/
apps/test/powersave/powersave.c:242:
undefined reference to `ARRAYSIZE'
Edit the powersave.c and change all ARRAYSIZE to ARRAY_SIZE. Then it should pass compilation.
In powersave.mk, there are 2 things defined as below. CYW94343WWCD1 is not in VALID_PLATFORMS, so you are seeing that issue. You can try adding whatever platform there for the build, but if the chipset really support that feature is different thing.
VALID_PLATFORMS := BCM943909* BCM943907* BCM943903* CYW943907* Quicksilver_EVL
INVALID_PLATFORMS := BCM943909QT
Hello,
Thanks for the reply.
I tried changing the makefile as below.
I am getting some other compilation errors. I even tried including header
file but no luck.
Added the platform BCM94343WWCD1 in the valid platform list.
Makefile:
Define as 1 if want to include WL commands into application
CONSOLE_ENABLE_WL := 0
VALID_PLATFORMS := BCM943909* BCM943907* BCM943903* CYW943907*
BCM4343W* BCM94343WWCD1*
INVALID_PLATFORMS := BCM943909QT
Compilation Error:
Making test.powersave-BCM94343WWCD1.elf
build/test.powersave-BCM94343WWCD1/libraries/App_powersave.a(powersave.o):
In function `startup_commands':
C:\Users\milan\Documents\WICED-Studio-6.0\43xxx_Wi-Fi/
apps/test/powersave/powersave.c:242:
undefined reference to `ARRAYSIZE'
tools/makefiles/wiced_elf.mk:315: recipe for target
'build/test.powersave-BCM94343WWCD1/binary/test.
powersave-BCM94343WWCD1.elf'
failed
Makefile:349: recipe for target 'main_app' failed
make.exe[1]: ***
[build/test.powersave-BCM94343WWCD1/binary/test.
powersave-BCM94343WWCD1.elf]
Error 1
make: *** Error 2
18:42:49 Build Finished (took 46s.418ms)
Do I need to so some more setting for this compatibility?
On Thu 15 Nov, 2018, 11:29 PM inoue_tomohiro_1742091 <
cool.milu69_3789331 wrote:
Hello,
Thanks for the reply.
I tried changing the makefile as below.
I am getting some other compilation errors. I even tried including header
file but no luck.
Added the platform BCM94343WWCD1 in the valid platform list.
Makefile:
Define as 1 if want to include WL commands into application
CONSOLE_ENABLE_WL := 0
VALID_PLATFORMS := BCM943909* BCM943907* BCM943903* CYW943907*
BCM4343W* BCM94343WWCD1*
INVALID_PLATFORMS := BCM943909QT
Compilation Error:
Making test.powersave-BCM94343WWCD1.elf
build/test.powersave-BCM94343WWCD1/libraries/App_powersave.a(powersave.o):
In function `startup_commands':
C:\Users\milan\Documents\WICED-Studio-6.0\43xxx_Wi-Fi/
apps/test/powersave/powersave.c:242:
undefined reference to `ARRAYSIZE'
Edit the powersave.c and change all ARRAYSIZE to ARRAY_SIZE. Then it should pass compilation.