Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
NaFi_2915566
Level 3
Level 3
First like received First like given

I defined a structure within our application DCT and increased DCT size accordingly.

There are no write commands for the application DCT area.

I added multiple lock/read/print/unlock cycles to make it is not an unlock

Problem:

  • the DCT contents are loaded correctly when I load the code via JTAG but some parts are changed after a reset. 
  • the changed values are always changed to the same values,which points to another part of the code overwriting application DCT
  • we have code that writes to DCT_WIFI_CONFIG_SECTION to update wifi credentials

Questions:

  1. are there any other changes needed besides updating dct.ld?  Based on where the the overwrite is happening, it s past the old DCT.
  2. read_lock / read_unlock should not change the contents, right?

dct.ld increased from 16k to 64k:

MEMORY

{

/*    DCT1_FLASH                 (rx)  : ORIGIN = 0x0, LENGTH = 16K */

    DCT1_FLASH                 (rx)  : ORIGIN = 0x0, LENGTH = 64K

}

application_dct.h (some names are obscured)

#define DCT_SCHEMA_VERSION     1

#define DCT_CONFIG_FILE_SIZE   (20*1024)

#define DCT_WIFI_FILE_SIZE     (2*1024)

pragma pack (1)

typedef struct

{

   //overall content

   uint32_t schemaVersion;                       // BUILD

   uint32_t dummyTop[7];                         // FFS

  

   // configuration.json

   uint32_t configJsonSize;                      // redundant size of string

   uint32_t dummyConfigJson[7];                  // FFS

   char     configJsonStr[DCT_CONFIG_FILE_SIZE]; // BUILD

  

   // wifi.json

   uint32_t wifiJsonSize;                        // redundant size of string

   uint32_t dummyWifiJson[7];                    // FFS

   char     wifiJsonStr[DCT_WIFI_FILE_SIZE];     // BUILD

} ...Dct_t;

#pragma pack ()

} ...Dct_t;

#pragma pack ()

application_dct.c

DEFINE_APP_DCT(...Dct_t)

{

   .schemaVersion   = DCT_SCHEMA_VERSION,

   .dummyTop        = {0,1,2,3,4,5,6},

   .configJsonSize  = 6,

   .dummyConfigJson = {0,7,8,9,0xA,0xB,0xC},

   .configJsonStr   = "config",

   .wifiJsonSize    = 4,

   .dummyWifiJson   = {0,0xD,0xE,0xF,1,2,3},

   .wifiJsonStr     = "wifi"

};

application

   ...Dct_t *...Dct=NULL;

during startup,the application runs the following code three times

   // First check DCT to see if it has a valid file

   wResult = wiced_dct_read_lock( (void**) &...Dct, WICED_TRUE, DCT_APP_SECTION, 0, sizeof( ...Dct_t ) );

   if ( wResult == WICED_SUCCESS)

   {

         WPRINT_APP_DEBUG( ( "APP DCT\n" ) );

         WPRINT_APP_DEBUG( ( " schemaVersion   : %lu\n",datablizzard2Dct->schemaVersion ) );

         DEBUG_HEX_DUMP    ( " dummyTop        :",datablizzard2Dct->dummyTop,7);

         WPRINT_APP_DEBUG( ( " configJsonSize  : %lu\n",datablizzard2Dct->configJsonSize ) );

         DEBUG_HEX_DUMP    ( " dummyConfigJson :",datablizzard2Dct->dummyConfigJson,7);

         WPRINT_APP_DEBUG( ( " configJsonStr   : %.10s\n",datablizzard2Dct->configJsonStr ) );

         WPRINT_APP_DEBUG( ( " wifiJsonSize    : %lu\n",datablizzard2Dct->wifiJsonSize ) );

         DEBUG_HEX_DUMP    ( " dummyWifiJson   :",datablizzard2Dct->dummyWifiJson,7);

         WPRINT_APP_DEBUG( ( " wifiJsonStr     : %.10s\n",datablizzard2Dct->wifiJsonStr ) );

      // done with DCT, close it

      wResult = wiced_dct_read_unlock( ...Dct, WICED_TRUE );

      if ( wResult != WICED_SUCCESS)

      {

         WPRINT_APP_ERROR( ( "%s wiced_dct_read_unlock failed: %u\n", __FUNCTION__, wResult) );

      }

      else

      {

         WPRINT_APP_DEBUG( ( "%s wiced_dct_read_unlock done\n", __FUNCTION__) );

      }        

   }  

the attached log file shows the correct DCT being printed 3 times.

then following a reset, some of the values are changed.

0 Likes
1 Solution
RaktimR_11
Moderator
Moderator
Moderator
500 replies posted 250 replies posted 100 replies posted

To increase the DCT, 3 files need to be modified,

1. In the DCT.ld (/43xxx_Wi-Fi/WICED/platform/MCU/BCM4390x/GCC/dct.ld) where the DCT1_FLASH LENGTH needs to be modified based on the required length.

2. In the waf_platform.h (/43xxx_Wi-Fi/WICED/platform/MCU/BCM4390x/WAF/waf_platform.h) file where the PLATFORM_DCT_COPY1_SIZE needs to be modified

3. The memory address bases need to be modified according to the memory requirement in either normal_image_defines.mk(/43xxx_Wi-Fi/platforms/CYW943907AEVAL1F/) or the OTA2_image_defines.mk based on the ota2 or production use-case.

View solution in original post

3 Replies
NaFi_2915566
Level 3
Level 3
First like received First like given

(10:11:03.566)

(10:11:03.566) Starting WICED vWiced_006.002.001.0002

(10:11:03.566) Platform DataBlizzard2_Rev_A initialised

(10:11:03.566) Started ThreadX v5.8

(10:11:03.566) Initialising NetX_Duo v5.10_sp3

(10:11:03.566) Creating Packet pools

(10:11:03.945) WLAN MAC Address : 10:98:C3:70:9C:1C<CR>

(10:11:03.945) WLAN Firmware    : wl0: May 15 2018 19:39:17 version 7.15.168.114 (r689934) FWID 01-d6f88905<CR>

(10:11:03.945) WLAN CLM         : API: 12.2 Data: 9.10.74 Compiler: 1.31.3 ClmImport: 1.36.3 Creation: 2018-05-15 19:33:15 <CR>

(10:11:03.945) Set UI State to 1

(10:11:03.945) start configuration thread

(10:11:03.945)   configuration thread started (5886836)

(10:11:03.945) APP DCT

(10:11:03.945)  schemaVersion   : 1

(10:11:03.945)  dummyTop        : [00000000,00000001,00000002,00000003,00000004,00000005,00000006,]

(10:11:03.945)  configJsonSize  : 6

(10:11:03.945)  dummyConfigJson : [00000000,00000007,00000008,00000009,0000000A,0000000B,0000000C,]

(10:11:03.945)  configJsonStr   : config

(10:11:03.945)  wifiJsonSize    : 4

(10:11:03.945)  dummyWifiJson   : [00000000,0000000D,0000000E,0000000F,00000001,00000002,00000003,]

(10:11:03.945)  wifiJsonStr     : wifi

(10:11:03.945) ParseWifiJson wiced_dct_read_unlock done

(10:11:03.945) APP DCT

(10:11:03.945)  schemaVersion   : 1

(10:11:03.945)  dummyTop        : [00000000,00000001,00000002,00000003,00000004,00000005,00000006,]

(10:11:03.945)  configJsonSize  : 6

(10:11:03.945)  dummyConfigJson : [00000000,00000007,00000008,00000009,0000000A,0000000B,0000000C,]

(10:11:03.945)  configJsonStr   : config

(10:11:03.945)  wifiJsonSize    : 4

(10:11:03.945)  dummyWifiJson   : [00000000,0000000D,0000000E,0000000F,00000001,00000002,00000003,]

(10:11:03.945)  wifiJsonStr     : wifi

(10:11:03.945) ParseWifiJson wiced_dct_read_unlock done

(10:11:03.945) APP DCT

(10:11:03.945)  schemaVersion   : 1

(10:11:03.945)  dummyTop        : [00000000,00000001,00000002,00000003,00000004,00000005,00000006,]

(10:11:03.945)  configJsonSize  : 6

(10:11:03.945)  dummyConfigJson : [00000000,00000007,00000008,00000009,0000000A,0000000B,0000000C,]

(10:11:03.945)  configJsonStr   : config

(10:11:03.945)  wifiJsonSize    : 4

(10:11:03.945)  dummyWifiJson   : [00000000,0000000D,0000000E,0000000F,00000001,00000002,00000003,]

(10:11:03.945)  wifiJsonStr     : wifi

(10:11:03.945) ParseWifiJson wiced_dct_read_unlock done

(10:11:03.945)

<<<<<<<<<<<<< MANUAL RESET >>>>>>>>>>>>>>>>

(10:11:11.315) Starting WICED vWiced_006.002.001.0002

(10:11:11.315) Platform DataBlizzard2_Rev_A initialised

(10:11:11.381) Started ThreadX v5.8

(10:11:11.381) Initialising NetX_Duo v5.10_sp3

(10:11:11.381) Creating Packet pools

(10:11:11.728) WLAN MAC Address : 10:98:C3:70:9C:1C<CR>

(10:11:11.728) WLAN Firmware    : wl0: May 15 2018 19:39:17 version 7.15.168.114 (r689934) FWID 01-d6f88905<CR>

(10:11:11.728) WLAN CLM         : API: 12.2 Data: 9.10.74 Compiler: 1.31.3 ClmImport: 1.36.3 Creation: 2018-05-15 19:33:15 <CR>

(10:11:11.728) Set UI State to 1

(10:11:11.728) start configuration thread

(10:11:11.728)   configuration thread started (5886836)

(10:11:11.728) APP DCT

(10:11:11.728)  schemaVersion   : 1

(10:11:11.728)  dummyTop        : [00000000,00000001,00000002,00000003,00000004,00000005,00000006,]

(10:11:11.728)  configJsonSize  : 6

(10:11:11.728)  dummyConfigJson : [00000000,00000007,00000008,00000009,0000000A,0000000B,0000000C,]

(10:11:11.728)  configJsonStr   : config

(10:11:11.728)  wifiJsonSize    : 3993371137

(10:11:11.728)  dummyWifiJson   : [EE062F51,F7FF3F91,F85DFFDE,BF00FB04,EE100000,F3C00F90,29002107,]

(10:11:11.728)  wifiJsonStr     :

(10:11:11.728) ParseWifiJson wiced_dct_read_unlock done

(10:11:11.728) APP DCT

(10:11:11.728)  schemaVersion   : 1

(10:11:11.728)  dummyTop        : [00000000,00000001,00000002,00000003,00000004,00000005,00000006,]

(10:11:11.728)  configJsonSize  : 6

(10:11:11.728)  dummyConfigJson : [00000000,00000007,00000008,00000009,0000000A,0000000B,0000000C,]

(10:11:11.728)  configJsonStr   : config

(10:11:11.728)  wifiJsonSize    : 3993371137

(10:11:11.728)  dummyWifiJson   : [EE062F51,F7FF3F91,F85DFFDE,BF00FB04,EE100000,F3C00F90,29002107,]

(10:11:11.728)  wifiJsonStr     :

(10:11:11.728) ParseWifiJson wiced_dct_read_unlock done

(10:11:11.728) APP DCT

(10:11:11.728)  schemaVersion   : 1

(10:11:11.728)  dummyTop        : [00000000,00000001,00000002,00000003,00000004,00000005,00000006,]

(10:11:11.728)  configJsonSize  : 6

(10:11:11.728)  dummyConfigJson : [00000000,00000007,00000008,00000009,0000000A,0000000B,0000000C,]

(10:11:11.728)  configJsonStr   : config

(10:11:11.728)  wifiJsonSize    : 3993371137

(10:11:11.728)  dummyWifiJson   : [EE062F51,F7FF3F91,F85DFFDE,BF00FB04,EE100000,F3C00F90,29002107,]

(10:11:11.728)  wifiJsonStr     :

(10:11:11.728) ParseWifiJson wiced_dct_read_unlock done

(10:11:11.728)

<<<<<<<<<<<<< MANUAL RESET >>>>>>>>>>>>>>>>

(10:11:20.716) Starting WICED vWiced_006.002.001.0002

(10:11:20.804) Platform DataBlizzard2_Rev_A initialised

(10:11:20.804) Started ThreadX v5.8

(10:11:20.804) Initialising NetX_Duo v5.10_sp3

(10:11:20.804) Creating Packet pools

(10:11:21.131) WLAN MAC Address : 10:98:C3:70:9C:1C<CR>

(10:11:21.131) WLAN Firmware    : wl0: May 15 2018 19:39:17 version 7.15.168.114 (r689934) FWID 01-d6f88905<CR>

(10:11:21.131) WLAN CLM         : API: 12.2 Data: 9.10.74 Compiler: 1.31.3 ClmImport: 1.36.3 Creation: 2018-05-15 19:33:15 <CR>

(10:11:21.131) Set UI State to 1

(10:11:21.131) start configuration thread

(10:11:21.131)   configuration thread started (5886836)

(10:11:21.131) APP DCT

(10:11:21.131)  schemaVersion   : 1

(10:11:21.131)  dummyTop        : [00000000,00000001,00000002,00000003,00000004,00000005,00000006,]

(10:11:21.131)  configJsonSize  : 6

(10:11:21.131)  dummyConfigJson : [00000000,00000007,00000008,00000009,0000000A,0000000B,0000000C,]

(10:11:21.131)  configJsonStr   : config

(10:11:21.131)  wifiJsonSize    : 3993371137

(10:11:21.131)  dummyWifiJson   : [EE062F51,F7FF3F91,F85DFFDE,BF00FB04,EE100000,F3C00F90,29002107,]

(10:11:21.131)  wifiJsonStr     :

(10:11:21.131) ParseWifiJson wiced_dct_read_unlock done

(10:11:21.131) APP DCT

(10:11:21.131)  schemaVersion   : 1

(10:11:21.131)  dummyTop        : [00000000,00000001,00000002,00000003,00000004,00000005,00000006,]

(10:11:21.131)  configJsonSize  : 6

(10:11:21.131)  dummyConfigJson : [00000000,00000007,00000008,00000009,0000000A,0000000B,0000000C,]

(10:11:21.131)  configJsonStr   : config

(10:11:21.131)  wifiJsonSize    : 3993371137

(10:11:21.131)  dummyWifiJson   : [EE062F51,F7FF3F91,F85DFFDE,BF00FB04,EE100000,F3C00F90,29002107,]

(10:11:21.131)  wifiJsonStr     :

(10:11:21.131) ParseWifiJson wiced_dct_read_unlock done

(10:11:21.131) APP DCT

(10:11:21.131)  schemaVersion   : 1

(10:11:21.131)  dummyTop        : [00000000,00000001,00000002,00000003,00000004,00000005,00000006,]

(10:11:21.131)  configJsonSize  : 6

(10:11:21.131)  dummyConfigJson : [00000000,00000007,00000008,00000009,0000000A,0000000B,0000000C,]

(10:11:21.131)  configJsonStr   : config

(10:11:21.131)  wifiJsonSize    : 3993371137

(10:11:21.131)  dummyWifiJson   : [EE062F51,F7FF3F91,F85DFFDE,BF00FB04,EE100000,F3C00F90,29002107,]

(10:11:21.131)  wifiJsonStr     :

(10:11:21.131) ParseWifiJson wiced_dct_read_unlock done

(10:11:21.131)

0 Likes
RaktimR_11
Moderator
Moderator
Moderator
500 replies posted 250 replies posted 100 replies posted

To increase the DCT, 3 files need to be modified,

1. In the DCT.ld (/43xxx_Wi-Fi/WICED/platform/MCU/BCM4390x/GCC/dct.ld) where the DCT1_FLASH LENGTH needs to be modified based on the required length.

2. In the waf_platform.h (/43xxx_Wi-Fi/WICED/platform/MCU/BCM4390x/WAF/waf_platform.h) file where the PLATFORM_DCT_COPY1_SIZE needs to be modified

3. The memory address bases need to be modified according to the memory requirement in either normal_image_defines.mk(/43xxx_Wi-Fi/platforms/CYW943907AEVAL1F/) or the OTA2_image_defines.mk based on the ota2 or production use-case.

this solved my problem, thanks

0 Likes