Antenna selection with mbt for BLE certification test?

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
user_108962310
Level 4
Level 4
10 likes received 10 likes given 5 likes given

In my hardware, I am using antenna "1" from the point of view of the wl tool, or WICED_ANTENNA_2 in the WWD enum parlance.
I need to run the test.bt_mfg_test app to do wireless certification. I am using a 4343W radio.
How can I set the antenna selection from the mbt tool to choose the correct antenna?

Also, I have seen some references to "BlueTool" software from Cypress that might be able start/stop the same tests that mbt does. Is that tool available for download anywhere?

0 Likes
1 Solution
Anonymous
Not applicable

It is not possible to select the antenna from the mbt tool.

Bluetool is an internal tool (atleast currently) and is not available for customers at the moment.

View solution in original post

0 Likes
1 Reply
Anonymous
Not applicable

It is not possible to select the antenna from the mbt tool.

Bluetool is an internal tool (atleast currently) and is not available for customers at the moment.

0 Likes