Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Anonymous
Not applicable

I try the aws shadow example in 3.5.2 and it worked fine .Now I want to add BLE function to the example.Here is my code:

/******************************************************

*               Function Definitions

******************************************************/

void application_start( void )

{

  wiced_result_t   ret = WICED_SUCCESS;

  int              connection_retries = 0;

  wiced_init( );

  ret = aws_app_init(&app_info);

  wiced_JSON_parser_register_callback(parse_json_shadow_status);

  wiced_gpio_input_irq_enable( SETUP_BUTTON, IRQ_TRIGGER_RISING_EDGE, setpoint_control_keypad_handler, NULL );

  wiced_gpio_init(USER_LED, OUTPUT_PUSH_PULL);

  do

  {

  ret = aws_mqtt_conn_open( app_info.mqtt_object, mqtt_connection_event_cb );

  connection_retries++ ;

  } while ( ( ret != WICED_SUCCESS ) && ( connection_retries < WICED_MQTT_CONNECTION_NUMBER_OF_RETRIES ) );

  aws_mqtt_app_publish( app_info.mqtt_object, WICED_MQTT_QOS_DELIVER_AT_LEAST_ONCE, (uint8_t*)app_info.shadow_state_topic, (uint8_t*)SHADOW_INIT ,sizeof(SHADOW_INIT) );

  wiced_rtos_delay_milliseconds( MQTT_DELAY_IN_MILLISECONDS * 2 );

  aws_mqtt_app_subscribe( app_info.mqtt_object, app_info.shadow_delta_topic , WICED_MQTT_QOS_DELIVER_AT_LEAST_ONCE );

/* Initialize Bluetooth controller and host stack */

wiced_bt_stack_init( ble_scan_management_callback, &wiced_bt_cfg_settings, wiced_bt_cfg_buf_pools );

while ( 1 )

    {

        /* Wait forever on wake semaphore until the wake button is pressed */

        wiced_rtos_get_semaphore( &app_info.wake_semaphore, WICED_NEVER_TIMEOUT );

        /* Toggle the LED */

        if ( strcasecmp( led_status, "ON" ) == 0 )

        {

            wiced_gpio_output_low( USER_LED );

            led_status = "OFF";

            strcpy(req_led_status, led_status);

            aws_mqtt_app_publish( app_info.mqtt_object, WICED_MQTT_QOS_DELIVER_AT_LEAST_ONCE, (uint8_t*)app_info.shadow_state_topic, (uint8_t*)SHADOW_PUBLISH_MESSAGE_STR_OFF_DESIRED_AND_REPORTED ,sizeof(SHADOW_PUBLISH_MESSAGE_STR_OFF_DESIRED_AND_REPORTED) );

        }

        else

        {

            wiced_gpio_output_high( USER_LED );

            led_status = "ON";

            strcpy(req_led_status, led_status);

            aws_mqtt_app_publish( app_info.mqtt_object, WICED_MQTT_QOS_DELIVER_AT_LEAST_ONCE, (uint8_t*)app_info.shadow_state_topic, (uint8_t*)SHADOW_PUBLISH_MESSAGE_STR_ON_DESIRED_AND_REPORTED ,sizeof(SHADOW_PUBLISH_MESSAGE_STR_ON_DESIRED_AND_REPORTED) );

        }

    }

}

After I set the cer/ private key/router config,I set the BLE as central too scan some peripheral device.But got error .Here is the information it print

[MQTT] Connecting to broker 52.77.134.96 ...

Thing Name:....

Shadow State Topic: $aws/thing...

Shadow Delta Topic: $aws/thing...

Reading the certificate and private key from DCT...

[MQTT] Connecting to MQTT Broker...

[MQTT] Successfully connected MQTT Broker

Publish SUCCEEDED for topic...

Subscribe SUCCEEDED for topic...

00020784 GKI_create_task func=0x803ddb9  id=1  name=BTU  stack=0x0  stackSize=6144

00020792 GKI_create_task func=0x8044465  id=0  name=HCISU  stack=0x0  stackSize=4096

00020800 GKI_create_task thread_id failed(8), HCISU!

00060905 GKI_exception(): Task State Table

00060909 GKI_exception 65524 getbuf: out of buffers

00064905 GKI_exception(): Task State Table

Who can tell me the reason?Thanks

1 Solution
Anonymous
Not applicable

Hi.

Did you check to make sure you have enough buffers allocated for BLE?

/*****************************************************************************

* wiced_bt_stack buffer pool configuration

*

* Configure buffer pools used by the stack

*

* Pools must be ordered in increasing buf_size.

* If a pool runs out of buffers, the next  pool will be used

*****************************************************************************/

const wiced_bt_cfg_buf_pool_t wiced_bt_cfg_buf_pools[WICED_BT_CFG_NUM_BUF_POOLS] =

{

/*  { buf_size, buf_count } */

    { 64,       4   },      /* Small Buffer Pool */

    { 360,      4   },      /* Medium Buffer Pool (used for HCI & RFCOMM control messages, min recommended size is 360) */

    { 360,      12  },      /* Large Buffer Pool  (used for HCI ACL messages) */

    { 360,      0   },      /* Extra Large Buffer Pool - Used for avdt media packets and miscellaneous (if not needed, set buf_count to 0) */

};

Also make sure you instantiate the BLE Stack first. Then you can try to bring up WiFi in STA mode. If that works fine, try MQTT. Please repurpose the ble_proximity_reporter as is. What I see in your code is just a wiced_bt_stack_init() ...

Also remember that the MQTT protocol needs a context of its own. You cannot expect a while(1) loop to share context with BLE. Have a network priority worker thread give context to MQTT (and not the main application).

Hope that helps!

Regards,

Manish

View solution in original post

2 Replies
Anonymous
Not applicable

Hi.

Did you check to make sure you have enough buffers allocated for BLE?

/*****************************************************************************

* wiced_bt_stack buffer pool configuration

*

* Configure buffer pools used by the stack

*

* Pools must be ordered in increasing buf_size.

* If a pool runs out of buffers, the next  pool will be used

*****************************************************************************/

const wiced_bt_cfg_buf_pool_t wiced_bt_cfg_buf_pools[WICED_BT_CFG_NUM_BUF_POOLS] =

{

/*  { buf_size, buf_count } */

    { 64,       4   },      /* Small Buffer Pool */

    { 360,      4   },      /* Medium Buffer Pool (used for HCI & RFCOMM control messages, min recommended size is 360) */

    { 360,      12  },      /* Large Buffer Pool  (used for HCI ACL messages) */

    { 360,      0   },      /* Extra Large Buffer Pool - Used for avdt media packets and miscellaneous (if not needed, set buf_count to 0) */

};

Also make sure you instantiate the BLE Stack first. Then you can try to bring up WiFi in STA mode. If that works fine, try MQTT. Please repurpose the ble_proximity_reporter as is. What I see in your code is just a wiced_bt_stack_init() ...

Also remember that the MQTT protocol needs a context of its own. You cannot expect a while(1) loop to share context with BLE. Have a network priority worker thread give context to MQTT (and not the main application).

Hope that helps!

Regards,

Manish

Anonymous
Not applicable

mkochhal wrote:

Hi.

Did you check to make sure you have enough buffers allocated for BLE?

/*****************************************************************************

* wiced_bt_stack buffer pool configuration

*

* Configure buffer pools used by the stack

*

* Pools must be ordered in increasing buf_size.

* If a pool runs out of buffers, the next  pool will be used

*****************************************************************************/

So how to calculate the number of required buf_count in various use cases?

I don't find any documentation about this and no response from the

forum about this question.

The above comment says "If a pool runs out of buffers, the next  pool will be used",

this makes developers hard to set exactly the required buffer count.

Usually, users just set a larger buf_count but the side effect is wasting memory.

0 Likes