十二月 21, 2020
10:48 PM
我使用的CY8CKIY-062-WiFi-BT板子连接电脑。发现在设备管理器中找不到Kitprog2或Kitprog3端口。PSoC programmer上也找不到。无法将程序上载到板子上。
请问应该如何解决?谢谢
标签
3 回复数
十二月 27, 2020
11:33 PM
1: 设备管理器下面显示的是什么?
如果显示的是感叹号,右击将minprog3的驱动重新安装。
The mprog3.inf file located at the following address is the driver file which need to be binded with miniprog3. This inf file points to sys file which is required for connecting miniprog3 to USB.
C:\Program Files\Cypress\Programmer\3.12\drivers\mprog3
2: 查看Kitprog的安装文档,确认是不是SW3的模式选择的有问题。
十二月 27, 2020
11:49 PM
谢谢
1. 设备管理器里面没有显示KitProg
2. 说明文档看过了,按下SW3但是显示状态的LED并没有变化
十二月 28, 2020
10:24 PM