Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
sayec_3752646
Level 1
Level 1

Hi All,

I am trying to port cyw43455 wifi/bt on imx8mevk. I am able to figure out dts node for bluetooth porting pins but confused when porting wifi related configurations.

Below are the pin and port details I am using

wifi --> sdio

BT --> UART2.

    

NET NAME

IMX8 Pin name

BT_REG_ONNAND_CLE
WL_REG_ONNAND_CE2_B
BT_HOST_WAKENAND_DQS
BT_DEV_WAKENAND_CE1_B
REF_CLK_32KGPIO1_IO00
SD1_CMDSD1_CMD
SD1_DATA0SD1_DATA0
SD1_DATA1SD1_DATA1
SD1_DATA2SD1_DATA2
SD1_DATA3SD1_DATA3
SD1_CLKSD1_CLK
UART2_RXDUART2_RXD
UART2_TXDUART2_TXD
UART2_CTSUART4_RXD
UART2_RTSUART4_TXD
SAI5_RXD1L4
SAI3_TXFSG3
SAI3_TXCC4
SAI3_TXDC3
SAI3_RXDF3

Here we are using both 1.8v for VIO and 3.3v for VBAT_LDO, but I don't have any clue how to configure VIO and VBAT in dts file. Please find attached dts prepared for above configuration. Please correct me if anything is wrong and help me how to add vio and vbat configuration in dts.

0 Likes
1 Solution
VinayakS_26
Moderator
Moderator
Moderator
100 replies posted 50 replies posted 25 replies posted

These properties are common to multiple MMC host controllers. Any host

that requires the respective functionality should implement them using

these definitions.

Interpreted by the OF core:

- reg: Registers location and length.

- interrupts: Interrupts used by the MMC controller.

Card detection:

If no property below is supplied, host native card detect is used.

Only one of the properties in this section should be supplied:

  - broken-cd: There is no card detection available; polling must be used.

  - cd-gpios: Specify GPIOs for card detection, see gpio binding

  - non-removable: non-removable slot (like eMMC); assume always present.

  - cd-post: postone card detect from start host for non-removable cards

     and let client driver to start it when ready

Optional properties:

- bus-width: Number of data lines, can be <1>, <4>, or <8>.  The default

  will be <1> if the property is absent.

- wp-gpios: Specify GPIOs for write protection, see gpio binding

- cd-inverted: when present, polarity on the CD line is inverted. See the note

  below for the case, when a GPIO is used for the CD line

- wp-inverted: when present, polarity on the WP line is inverted. See the note

  below for the case, when a GPIO is used for the WP line

- disable-wp: When set no physical WP line is present. This property should

  only be specified when the controller has a dedicated write-protect

  detection logic. If a GPIO is always used for the write-protect detection

  logic it is sufficient to not specify wp-gpios property in the absence of a WP

  line.

- max-frequency: maximum operating clock frequency

- no-1-8-v: when present, denotes that 1.8v card voltage is not supported on

  this system, even if the controller claims it is.

- cap-sd-highspeed: SD high-speed timing is supported

- cap-mmc-highspeed: MMC high-speed timing is supported

- sd-uhs-sdr12: SD UHS SDR12 speed is supported

- sd-uhs-sdr25: SD UHS SDR25 speed is supported

- sd-uhs-sdr50: SD UHS SDR50 speed is supported

- sd-uhs-sdr104: SD UHS SDR104 speed is supported

- sd-uhs-ddr50: SD UHS DDR50 speed is supported

- cap-power-off-card: powering off the card is safe

- cap-sdio-irq: enable SDIO IRQ signalling on this interface

- full-pwr-cycle: full power cycle of the card is supported

- mmc-ddr-1_8v: eMMC high-speed DDR mode(1.8V I/O) is supported

- mmc-ddr-1_2v: eMMC high-speed DDR mode(1.2V I/O) is supported

- mmc-hs200-1_8v: eMMC HS200 mode(1.8V I/O) is supported

- mmc-hs200-1_2v: eMMC HS200 mode(1.2V I/O) is supported

- mmc-hs400-1_8v: eMMC HS400 mode(1.8V I/O) is supported

- mmc-hs400-1_2v: eMMC HS400 mode(1.2V I/O) is supported

- dsr: Value the card's (optional) Driver Stage Register (DSR) should be

  programmed with. Valid range: [0 .. 0xffff].

*NOTE* on CD and WP polarity. To use common for all SD/MMC host controllers line

polarity properties, we have to fix the meaning of the "normal" and "inverted"

line levels. We choose to follow the SDHCI standard, which specifies both those

lines as "active low." Therefore, using the "cd-inverted" property means, that

the CD line is active high, i.e. it is high, when a card is inserted. Similar

logic applies to the "wp-inverted" property.

CD and WP lines can be implemented on the hardware in one of two ways: as GPIOs,

specified in cd-gpios and wp-gpios properties, or as dedicated pins. Polarity of

dedicated pins can be specified, using *-inverted properties. GPIO polarity can

also be specified using the OF_GPIO_ACTIVE_LOW flag. This creates an ambiguity

in the latter case. We choose to use the XOR logic for GPIO CD and WP lines.

This means, the two properties are "superimposed," for example leaving the

OF_GPIO_ACTIVE_LOW flag clear and specifying the respective *-inverted

property results in a double-inversion and actually means the "normal" line

polarity is in effect.

Optional SDIO properties:

- keep-power-in-suspend: Preserves card power during a suspend/resume cycle

- enable-sdio-wakeup: Enables wake up of host system on SDIO IRQ assertion

- pm-ignore-notify: Ignore mmc PM notify. This will prevent MMC core automatically

    to re-detect cards after sysem resume back.

MMC power sequences:

--------------------

System on chip designs may specify a specific MMC power sequence. To

successfully detect an (e)MMC/SD/SDIO card, that power sequence must be

maintained while initializing the card.

Optional property:

- mmc-pwrseq: phandle to the MMC power sequence node. See "mmc-pwrseq-*"

for documentation of MMC power sequence bindings.

Use of Function subnodes

------------------------

On embedded systems the cards connected to a host may need additional

properties. These can be specified in subnodes to the host controller node.

The subnodes are identified by the standard 'reg' property.

Which information exactly can be specified depends on the bindings for the

SDIO function driver for the subnode, as specified by the compatible string.

Required host node properties when using function subnodes:

- #address-cells: should be one. The cell is the slot id.

- #size-cells: should be zero.

Required function subnode properties:

- compatible: name of SDIO function following generic names recommended practice

- reg: Must contain the SDIO function number of the function this subnode

       describes. A value of 0 denotes the memory SD function, values from

       1 to 7 denote the SDIO functions.

Examples

--------

Basic example:

sdhci@ab000000 {

compatible = "sdhci";

reg = <0xab000000 0x200>;

interrupts = <23>;

bus-width = <4>;

cd-gpios = <&gpio 69 0>;

cd-inverted;

wp-gpios = <&gpio 70 0>;

max-frequency = <50000000>;

keep-power-in-suspend;

enable-sdio-wakeup;

mmc-pwrseq = <&sdhci0_pwrseq>

}

Example with sdio function subnode:

mmc3: mmc@01c12000 {

#address-cells = <1>;

#size-cells = <0>;

pinctrl-names = "default";

pinctrl-0 = <&mmc3_pins_a>;

vmmc-supply = <&reg_vmmc3>;

bus-width = <4>;

non-removable;

mmc-pwrseq = <&sdhci0_pwrseq>

status = "okay";

brcmf: bcrmf@1 {

reg = <1>;

compatible = "brcm,bcm43xx-fmac";

interrupt-parent = <&pio>;

interrupts = <10 8>; /* PH10 / EINT10 */

interrupt-names = "host-wake";

};

};

View solution in original post

2 Replies
VinayakS_26
Moderator
Moderator
Moderator
100 replies posted 50 replies posted 25 replies posted

You could check the kernel documentation in the kernel source tree.

The documentation will be in Documenation/devicetree/bindings/mmc/mmc.txt

Cypress Linux WiFi Driver Release (FMAC) [2018-07-16]

The above link will the kernel source for 4.1.15_2.0.0. Hope this gives an insight into it.

VinayakS_26
Moderator
Moderator
Moderator
100 replies posted 50 replies posted 25 replies posted

These properties are common to multiple MMC host controllers. Any host

that requires the respective functionality should implement them using

these definitions.

Interpreted by the OF core:

- reg: Registers location and length.

- interrupts: Interrupts used by the MMC controller.

Card detection:

If no property below is supplied, host native card detect is used.

Only one of the properties in this section should be supplied:

  - broken-cd: There is no card detection available; polling must be used.

  - cd-gpios: Specify GPIOs for card detection, see gpio binding

  - non-removable: non-removable slot (like eMMC); assume always present.

  - cd-post: postone card detect from start host for non-removable cards

     and let client driver to start it when ready

Optional properties:

- bus-width: Number of data lines, can be <1>, <4>, or <8>.  The default

  will be <1> if the property is absent.

- wp-gpios: Specify GPIOs for write protection, see gpio binding

- cd-inverted: when present, polarity on the CD line is inverted. See the note

  below for the case, when a GPIO is used for the CD line

- wp-inverted: when present, polarity on the WP line is inverted. See the note

  below for the case, when a GPIO is used for the WP line

- disable-wp: When set no physical WP line is present. This property should

  only be specified when the controller has a dedicated write-protect

  detection logic. If a GPIO is always used for the write-protect detection

  logic it is sufficient to not specify wp-gpios property in the absence of a WP

  line.

- max-frequency: maximum operating clock frequency

- no-1-8-v: when present, denotes that 1.8v card voltage is not supported on

  this system, even if the controller claims it is.

- cap-sd-highspeed: SD high-speed timing is supported

- cap-mmc-highspeed: MMC high-speed timing is supported

- sd-uhs-sdr12: SD UHS SDR12 speed is supported

- sd-uhs-sdr25: SD UHS SDR25 speed is supported

- sd-uhs-sdr50: SD UHS SDR50 speed is supported

- sd-uhs-sdr104: SD UHS SDR104 speed is supported

- sd-uhs-ddr50: SD UHS DDR50 speed is supported

- cap-power-off-card: powering off the card is safe

- cap-sdio-irq: enable SDIO IRQ signalling on this interface

- full-pwr-cycle: full power cycle of the card is supported

- mmc-ddr-1_8v: eMMC high-speed DDR mode(1.8V I/O) is supported

- mmc-ddr-1_2v: eMMC high-speed DDR mode(1.2V I/O) is supported

- mmc-hs200-1_8v: eMMC HS200 mode(1.8V I/O) is supported

- mmc-hs200-1_2v: eMMC HS200 mode(1.2V I/O) is supported

- mmc-hs400-1_8v: eMMC HS400 mode(1.8V I/O) is supported

- mmc-hs400-1_2v: eMMC HS400 mode(1.2V I/O) is supported

- dsr: Value the card's (optional) Driver Stage Register (DSR) should be

  programmed with. Valid range: [0 .. 0xffff].

*NOTE* on CD and WP polarity. To use common for all SD/MMC host controllers line

polarity properties, we have to fix the meaning of the "normal" and "inverted"

line levels. We choose to follow the SDHCI standard, which specifies both those

lines as "active low." Therefore, using the "cd-inverted" property means, that

the CD line is active high, i.e. it is high, when a card is inserted. Similar

logic applies to the "wp-inverted" property.

CD and WP lines can be implemented on the hardware in one of two ways: as GPIOs,

specified in cd-gpios and wp-gpios properties, or as dedicated pins. Polarity of

dedicated pins can be specified, using *-inverted properties. GPIO polarity can

also be specified using the OF_GPIO_ACTIVE_LOW flag. This creates an ambiguity

in the latter case. We choose to use the XOR logic for GPIO CD and WP lines.

This means, the two properties are "superimposed," for example leaving the

OF_GPIO_ACTIVE_LOW flag clear and specifying the respective *-inverted

property results in a double-inversion and actually means the "normal" line

polarity is in effect.

Optional SDIO properties:

- keep-power-in-suspend: Preserves card power during a suspend/resume cycle

- enable-sdio-wakeup: Enables wake up of host system on SDIO IRQ assertion

- pm-ignore-notify: Ignore mmc PM notify. This will prevent MMC core automatically

    to re-detect cards after sysem resume back.

MMC power sequences:

--------------------

System on chip designs may specify a specific MMC power sequence. To

successfully detect an (e)MMC/SD/SDIO card, that power sequence must be

maintained while initializing the card.

Optional property:

- mmc-pwrseq: phandle to the MMC power sequence node. See "mmc-pwrseq-*"

for documentation of MMC power sequence bindings.

Use of Function subnodes

------------------------

On embedded systems the cards connected to a host may need additional

properties. These can be specified in subnodes to the host controller node.

The subnodes are identified by the standard 'reg' property.

Which information exactly can be specified depends on the bindings for the

SDIO function driver for the subnode, as specified by the compatible string.

Required host node properties when using function subnodes:

- #address-cells: should be one. The cell is the slot id.

- #size-cells: should be zero.

Required function subnode properties:

- compatible: name of SDIO function following generic names recommended practice

- reg: Must contain the SDIO function number of the function this subnode

       describes. A value of 0 denotes the memory SD function, values from

       1 to 7 denote the SDIO functions.

Examples

--------

Basic example:

sdhci@ab000000 {

compatible = "sdhci";

reg = <0xab000000 0x200>;

interrupts = <23>;

bus-width = <4>;

cd-gpios = <&gpio 69 0>;

cd-inverted;

wp-gpios = <&gpio 70 0>;

max-frequency = <50000000>;

keep-power-in-suspend;

enable-sdio-wakeup;

mmc-pwrseq = <&sdhci0_pwrseq>

}

Example with sdio function subnode:

mmc3: mmc@01c12000 {

#address-cells = <1>;

#size-cells = <0>;

pinctrl-names = "default";

pinctrl-0 = <&mmc3_pins_a>;

vmmc-supply = <&reg_vmmc3>;

bus-width = <4>;

non-removable;

mmc-pwrseq = <&sdhci0_pwrseq>

status = "okay";

brcmf: bcrmf@1 {

reg = <1>;

compatible = "brcm,bcm43xx-fmac";

interrupt-parent = <&pio>;

interrupts = <10 8>; /* PH10 / EINT10 */

interrupt-names = "host-wake";

};

};